Skip to main content
adityapandey3121992
Associate
Aug 1, 2014 11:45 AM UTC
Question

Camera interface firmware size in SRAM

Posted on August 01, 2014 at 13:45

Sir,

    I want to interface camera module that gives throughput of 28Mbps, & I want to interface it to STM32F207.

The same data is to be sent to wifi module using USB 2.0 by making STM32F207 as a host.

For this I want to know the firmware size that would be & also would there be sufficient SRAM available for loading wifi drivers?

Regards

Aditya

#dcmi-stm32f207
This topic has been closed for replies.

6 replies

Tesla DeLorean
Guru
Aug 1, 2014 2:26 PM UTC
Posted on August 01, 2014 at 16:26

Does the WiFi driver need to load into SRAM? What's you experience with this driver on other platforms you've used it on? What does it need there? Have you written many USB Host drivers?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
adityapandey3121992
Associate
Aug 5, 2014 7:15 AM UTC
Posted on August 05, 2014 at 09:15

Is STMF20 UVC compliant?

Tesla DeLorean
Guru
Aug 5, 2014 11:50 AM UTC
Posted on August 05, 2014 at 13:50

It's not a host example ST typically provides. The data rate you indicate suggests you'd need an external USB 2.0 HS PHY

If you don't have any experience writing USB host drivers, this probably isn't the platform to learn on.
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
adityapandey3121992
Associate
Aug 6, 2014 6:49 AM UTC
Posted on August 06, 2014 at 08:49

Dear Clive,

             I am a Hardware Engineer beginner & dont have any experiance regarding USB or any other interfaces.

All i need to do is to Interface camera module with resolution 1280X720p @ 30fps data stream (DVP interface) with STM32F207 & make it Wifi.

For this I am asking what would be easier for me,whether to use 54Mbps wifi module with SDIO interface or a wifi module with USB interface.

What all parameters would I need to look at? Please guide me.

adityapandey3121992
Associate
Aug 8, 2014 6:03 AM UTC
Posted on August 08, 2014 at 08:03

I need timing analysis of DVP DCMI to find rise time,fall time, setup time, hold time required for camera output to support the compatibility with STM32F207. Please give me the link of document. Regards Aditya,

adityapandey3121992
Associate
Aug 11, 2014 6:29 AM UTC
Posted on August 11, 2014 at 08:29

I need timing analysis literature of DVP DCMI to find rise time,fall time, setup time, hold time required for camera output to support the compatibility with STM32F207. Please give me the link of document.