Skip to main content
Spencer_0
Associate
May 9, 2021
Question

Camera initialization bug: use uninitialized field DMA_Handle of hDcmiEval in application Camera_To_USBDisk

The field DMA_Handle of the local data pointer phdcmi, which points to a global struct variable hDcmiEval, is not initialized in the function BSP_CAMERA_Init (from the file STM32Cube_FW_F4_V1.25.0/Drivers/BSP/STM32469I_EVAL/stm32469i_eval_camera.c).

uint8_t BSP_CAMERA_Init(uint32_t Resolution)
{
 DCMI_HandleTypeDef *phdcmi;
 uint8_t status = CAMERA_ERROR;
 
 /* Get the DCMI handle structure */
 phdcmi = &hDcmiEval;
 
 /*** Configures the DCMI to interface with the camera module ***/
 /* DCMI configuration */
 phdcmi->Init.CaptureRate = DCMI_CR_ALL_FRAME;
 phdcmi->Init.HSPolarity = DCMI_HSPOLARITY_HIGH;
 phdcmi->Init.SynchroMode = DCMI_SYNCHRO_HARDWARE;
 phdcmi->Init.VSPolarity = DCMI_VSPOLARITY_HIGH;
 phdcmi->Init.ExtendedDataMode = DCMI_EXTEND_DATA_8B;
 phdcmi->Init.PCKPolarity = DCMI_PCKPOLARITY_RISING;
 
 phdcmi->Instance = DCMI;
 
 /* Configure IO functionalities for CAMERA detect pin */
 BSP_IO_Init();
 /* Apply Camera Module hardware reset */
 BSP_CAMERA_HwReset();
...
}

In the function HAL_DCMI_Start_DMA (from the file STM32Cube_FW_F4_V1.25.0/Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_dcmi.c), the DMA_Handle field is used to store function pointers.

HAL_StatusTypeDef HAL_DCMI_Start_DMA(DCMI_HandleTypeDef* hdcmi, uint32_t DCMI_Mode, uint32_t pData, uint32_t Length)
{
 /* Initialize the second memory address */
 uint32_t SecondMemAddress = 0U;
 
 /* Check function parameters */
 assert_param(IS_DCMI_CAPTURE_MODE(DCMI_Mode));
 
 /* Process Locked */
 __HAL_LOCK(hdcmi);
 
 /* Lock the DCMI peripheral state */
 hdcmi->State = HAL_DCMI_STATE_BUSY;
 
 /* Enable DCMI by setting DCMIEN bit */
 __HAL_DCMI_ENABLE(hdcmi);
 
 /* Configure the DCMI Mode */
 hdcmi->Instance->CR &= ~(DCMI_CR_CM);
 hdcmi->Instance->CR |= (uint32_t)(DCMI_Mode);
 
 /* Set the DMA memory0 conversion complete callback */
 hdcmi->DMA_Handle->XferCpltCallback = DCMI_DMAXferCplt;
 
 /* Set the DMA error callback */
 hdcmi->DMA_Handle->XferErrorCallback = DCMI_DMAError;
 
 /* Set the dma abort callback */
 hdcmi->DMA_Handle->XferAbortCallback = NULL;
...
}

However, DMA_Handle points to the memory address 0x0000_0000, which is a invalid memory address.

In ARM Cortex-M4 MCUs, the code starts 0x800_0000. 

I am confused why this application runs well and does not crash. Is address 0x0000_0000 a valid memory address?

This topic has been closed for replies.

5 replies

Spencer_0
Spencer_0Author
Associate
May 10, 2021

The Camera_to_USBDisk application I use is in STM32F469I-EVAL, which belongs to STM32Cube_FW_F4_V1.25.0.

Does anybody can fix this bug?

ST Technical Moderator
May 18, 2021

Hello @Spencer_0​ ,

Let me first welcome you to the STM32 Community :)

I added the adequate topics to your question in order to increase its chance to be reviewed by our experts.

Hello @Walid ZRELLI​ ,

Can you please have a look at this post and confirm this issue ?

Thanks

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Walid ZRELLI
Visitor II
May 19, 2021

Hello @Spencer_0​ ,

In case of using DCMI_DOUBLE_BUFFER mode, the second memory address will be updated as follows:

SecondMemAddress = (uint32_t)(pData + (4U*hdcmi->XferSize)) ;

You could check the HAL_DCMI_Start_DMA() funtion.

So, there is no bug to fix.

With Regards,

Walid.

Spencer_0
Spencer_0Author
Associate
May 21, 2021

Hello @Walid ZRELLI​ , thanks for your reply.

I use the gdb to debug the application, and I find that the application doesn't use the DCMI_DOUBLE_BUFFER mode in my case.

The execution trace is here:

#0 HAL_DCMI_Start_DMA (hdcmi=0x200020e4 <hDcmiEval>, DCMI_Mode=0x0, pData=0xc0177000, Length=0x2580) at ../../../Drivers/STM32F4xx_HAL_Driver/Src/stm32f4xx_hal_dcmi.c:385
/* The program does not take the branch that uses the DCMI_DOUBLE_BUFFER mode here */
#1 0x0801012a in BSP_CAMERA_ContinuousStart (buff=0xc0177000 "\265\372\200") at ../../../Drivers/BSP/STM32469I_EVAL/stm32469i_eval_camera.c:276
#2 0x0802f15a in Camera_Init () at ../../Src/main.c:288
#3 0x0802f762 in main () at ../../Src/main.c:354

Apparently, if the application doesn't use the DCMI_DOUBLE_BUFFER mode, the address is still not transformed, and the pointer`hdcmi->DMA_Handle` points to the address 0x0000_0000.

So I believe that it is still an uninitialized field bug.

However, the picture captured by the Camera is always blank in my case. I wonder that if the proper execution flow should take the DCMI_DOUBLE_BUFFER mode branch. Otherwise the image captured by the camera is blank.

With kind regards,

Spencer Zhou

Spencer_0
Spencer_0Author
Associate
May 21, 2021

Thanks for your help @Imen DAHMEN​ :grinning_face: