Skip to main content
GMair
Associate II
September 24, 2020
Question

Build of TouchGFX with CubeIDE causes error messages everytime

Hi,

I try to build a TouchGFX project with the CubeIDE but during compilation I always get weird errror messages like that:

./TouchGFX/touchgfx/os/OSWrappers.cpp:1:10: fatal error: touchgfx/framework/include/touchgfx/hal/OSWrappers.hpp: No such file or directory

This file is definitely in the project (just like the others which create errors as well). The shortkey F3 guides me to the file. So CubeIDE in principle knows where to find it.

I already included the path - see attachment.

I'm using CubeIDE1.4.2 and TouchGFX 4.13. I know that they are not compatibel but I can't open TouchGFX 4.14. Neither manually nor automatically.

Thanks

Gerhard

This topic has been closed for replies.

16 replies

GMair
GMairAuthor
Associate II
October 6, 2020

Hello, Alexandre,

I tried your recommendation to create the project with CubeMX but I get the same errors just like TSchr.1.

Finally I downgraded CubeIDE to version 1.2.0. In combination with TouchGFX 4.13 I'm able to build the project in CubeIDE when

following the instructions from Karl Yamashita: https://www.youtube.com/watch?v=12KXreXaLp0

Best Regards

Gerhard

GMair
GMairAuthor
Associate II
October 6, 2020

When generating a project with CubeMX I get the same errors like doing it with CubeIDE.

Finally I downgraded CubeIDE to version 1.2.0. (using it with TouchGFX 4.13)

I followed the steps described in this video: https://www.youtube.com/watch?v=12KXreXaLp0

Then I'm able to build and debug the project.

Alexandre RENOUX
Visitor II
October 7, 2020

@GMair​ 

So you have missing files errors ? And you refreshed your project like TSchr.1 did ?

/Alexandre

GMair
GMairAuthor
Associate II
October 12, 2020

sorry I can't remember and I deleted the project since it did not work.