Build For Internal SRAM
- 3 replies
- 1581 views
Hi,
I am trying to reconfigure my project based off the STM32H750B-DK to run on the same part but from a custom PCB. I am using IAR and EWARM. I have configured my icf file based on what I would like for a memory map. The project builds okay, and I can verify what I am looking for with the map file, but for some reason after flashing the board my device screen is pure white (as if it was looking at initialized memory). Is there something in a source file that could be fighting with what I am trying to tell the linker/locator to do or am I missing a MAKE option? I have attached two map files to this message. The first map file is for an external SRAM build and uses the linker script included with the project; this is the working version. I have another map file which is using my custom linker script to build for internal SRAM (this version gives the white screen). Any help with this would be greatly appreciated.