Skip to main content
PBull
Associate II
Nov 16, 2022 12:26 PM UTC
Question

Bug with Graph / Histogram

Hello,

Coudn't find a Bugtracker, so I posted it here.

I use a static graph in my project, but after some time (adding other stuff) the TouchGFX-Designer (4.20) creates incomplete code:

This happend several times, only fix is to remove and add a new diagram.

This is the generated code:

0693W00000WIVwyQAH.pngThis is how it should be looking:

0693W00000WIVxSQAX.pngFurthermore, the Bar-Offset from Histogram, never appears in the generated Base Class.

0693W00000WIVzOQAX.png

This topic has been closed for replies.

4 replies

Yoann KLEIN
ST Employee
Nov 16, 2022 12:39 PM UTC

Hello @PBull​ ,

What are you adding exactly before noticing those issues in your code ?

If you want to access the bar offset parameter from your code, you can the setBarOffset() or getBarOffset() functions from this class.

/Yoann

Yoann KLEINST Software Developer | TouchGFX
PBull
PBullAuthor
Associate II
Nov 16, 2022 1:08 PM UTC

Hello Yoann,

sorry I'm not sure when this happens, coundn't find a way to reproduce it, but it happend several times.

I have three custom containers, each with a different Histogram, if this bug occur, the code is missing on all three of them. A new code generation doesn't help.

But I'll keep watching!

The setBarOffset() works well, if I add it manually, but it would be better if the Designer would do this for me ;)

Yoann KLEIN
ST Employee
Nov 16, 2022 1:30 PM UTC

Alright, please let me know if you figure out the cause of this bug, otherwise it will be hard to reproduce.

/Yoann

Yoann KLEINST Software Developer | TouchGFX
franck23
Associate III
Mar 27, 2023 10:11 AM UTC

Hi,

The Histogram Bar Offset do not appear in the generated code for me neither.

I add it manually in my code.

Color, Bar Width, and Baseline code is generated as expect.

TouchGFX 4.21.1