Skip to main content
SimonF
Senior
November 19, 2020
Solved

[BUG : STM32CubeProgrammer 2.6.0] Space in "Program Files" makes external loader loading failing

Hello,

I cannot use correctly TouchGFX Designer. When I use "run Target", when arriving at the step of stmCubeProgrammer, I have this issue :

...
-------------------------------------------------------------------
 STM32CubeProgrammer v2.6.0 
 -------------------------------------------------------------------
 
 Error: External loader c:\program cannot be loaded.
 Error: External loader files\stmicroelectronics\stm32cube\stm32cubeprogrammer\bin\externalloader\n25q128a_stm32469i-disco.stldr cannot be loaded.
 ST-LINK SN : 066EFF3530384E5043221930
 ST-LINK FW : V2J36M26
 Board : 32F469IDISCOVERY
 Voltage : 3.24V
 SWD freq : 4000 KHz
 Connect mode: Normal
 Reset mode : Software reset
 Device ID : 0x434
 Revision ID : Rev A
 Device name : STM32F469xx/F467xx
 Flash size : 2 MBytes
 Device type : MCU
 Device CPU : Cortex-M4
....

As you can see the path for the external loader path is splited in 2 parts because of the space in "Program Files". It seems that I am the only one with this issue ? I did not have this issue with the previous release of TouchGFX.

This topic has been closed for replies.
Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
December 17, 2020

Hi @Svenn Dahlstrom​ ,

CubeProgrammer team is fixing this, but in the meantime you can either use 2.5 and be happy, or.... i'm publishing a known issue for cubeprogrammer 2.6 to make it work with TouchGFX makefiles (which works since its from command-line as you mention).

/Martin

21 replies

Martin KJELDSEN
Principal III
November 19, 2020

Hi, i'll investigate if this is an issue with CubeProgrammer 2.6.0. That seems to be an internal error message.

/Martin

Uwe Bonnes
Chief
November 19, 2020

<sarcasme> Spaces and backslashes in filennames are such a great achievment</sarcasme>

SimonF
SimonFAuthor
Senior
November 19, 2020

@Martin KJELDSEN​ , I updated CubeProgrammer because I thought it was the issue. Thus, I had the same problem with previous release of CubeProgrammer.

I also reinstalled TouchGFX to the default folder just in case ^^

Martin KJELDSEN
Principal III
November 20, 2020

Oh, okay! That's really strange. There must be an internal refernce in cubeprogrammer to the loader files (stldr) but it fails because its inside program files. That's never been a problem here. I have 32-bit and 64-bit versions installed in both program files and program files (x86)

SimonF
SimonFAuthor
Senior
November 20, 2020

Do you mean that I am the "only" one having this issue ?

Can I test something to resolve this issue then ? Reinstall something with a previous release, or something else ?

Thank you.

Martin KJELDSEN
Principal III
November 20, 2020

​It's not something I've heard about before, no, hmm. I'm not an expert on CubeProgrammer to be honest.

I've added the CubeProgrammer topic to the post. Let's see if we can get some answers.

/Martin

Martin KJELDSEN
Principal III
November 20, 2020

I added this post to the STM32CubeProgrammer community as well

SimonF
SimonFAuthor
Senior
November 20, 2020

For the people more aware of STM32CubeProgrammer side. When using with the GUI (ie not with TouchGFX), I have no problem to add the external loader (by checking the right light under the "External loaders" menu) when connecting to the board. And thus, I can flash successfully the binary created by TouchGFX and I have the correct interface I have designed.

SimonF
SimonFAuthor
Senior
November 24, 2020

Hello @Martin KJELDSEN​ ,

I used the STM32CubeProgrammer CLI to test if it is TouchGFX related. And it is not. I have the same problem. Strangly, as I said, I don't seem to have the problem when using the CubeProgrammer GUI.

Should I create a new topic because it has nothing to do with TouchGFX ?

SimonF
SimonFAuthor
Senior
November 24, 2020

I confirm it works perfectly with STM32CubeProgrammer 2.5.0

Martin KJELDSEN
Principal III
November 25, 2020

So you're saying it works fine with the GUI, but not with the CLI? I think that since you added the topic CubeProgrammer to this post, it should be fine. Maybe we'll get some attention from people. I'll try to do some tests here, because i've never seen it before.

 

/Martin

SimonF
SimonFAuthor
Senior
November 25, 2020

Yes, I confirm that with STM32CubeProgrammer GUI in 2.6.0, I select the external Loader, I connect with the st-link to the board. I select the target.hex file and I download it in the MCU. The UI is then working correctly.

It doesn't not work if I use TouchGFX to flash : the display is completly "bugged". I mean : I download the Clock example and I see the form of the second and minute hands but it is wrong color and noisy.

Houda GHABRI
ST Employee
November 27, 2020

Hi @SimonF​ ,

I confirm , this is a known limitation with the space in the paths.

To resolve this problem, you can modify your command to directly call the external loader file, so you use externalloader\n25q128a_stm32469i-disco.stldr instead of the full path.

I hope this will help you.

Houda

SimonF
SimonFAuthor
Senior
November 27, 2020

Hello @Houda GHABRI​ ,

To avoid this problem, I went back to STM32CubeProgrammer 2.5.0 ! Isn't it strange that when updating from 2.5 to 2.6, there is a new limitation about spaces ? ^^'

Thank you for posting a workaround for people that really need the 2.6.0 version.

MLec
Visitor II
November 30, 2020

Hi. I confirm same behavior on my side.

Also worked worked with STM32CubeProgrammer 2.5.0.