Associate III
Nov 20, 2020 2:01 AM UTC
Question
BUG? Scrollable container/Dynamic graph crashes simulator (and hardware) - with no extra code.
- 4 replies
- 1442 views
This is an update to the question I asked earlier, but now I've reduced it to something that is creatable entierly in the Designer (in less than a minute!)
Create screen1 and add a scrollable container and a dynamic graph in this container, both 1200 pixels. choose the generate random values option.
Create screen2 with 10 lables and a button. Make the button swap to Screen1. Make this the startup screen.
Run - and crash!
Ive added the designer file so you can re create it. - just open and run in the simulator!
thanks Mark