Skip to main content
brianshankland9
Associate III
Feb 26, 2019 3:16 PM UTC
Solved

Bug Report for Designer assing in multiple textbuffers for wildcard (4.10.0)

I created a custom container in which I placed a scrollwheel.

I added in the item template and selected item template both of which use text with wildcard placements.

The problem arises when I select these text widgets to use a wildcard buffer at which point multiple identically named buffers are defined in the controls base class which cause the compiler to fail.

I have replicated in a small project whch I can zip and email if you say who can deal with this.

This topic has been closed for replies.
Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
Mar 7, 2019 9:10 AM UTC

Hi @brianshankland9​,

This issue was present in 4.10.0 but has been fixed in 4.11.0.

2 replies

Martin KJELDSEN
Principal III
Mar 6, 2019 12:43 PM UTC

Hi @brianshankland9​,

Please share the project with me. How do you want to do it? Which version of TouchGFX is this?

(Thanks for your report. I'll gladly check to see if you're right)

Best regards,

Martin

Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
Mar 7, 2019 9:10 AM UTC

Hi @brianshankland9​,

This issue was present in 4.10.0 but has been fixed in 4.11.0.