Skip to main content
MDi D.1
Associate II
Sep 15, 2022 12:06 PM UTC
Question

BUG on touch GFX4.20.0

If you choose the object "Static Graph"

and in this order:

set Y-axis Range Min = 60

set X-axis Range Min = 0

set X-axis Range Max = 8

click with the mouse into the Y-axis Range Min box

The value into the X-axis Range Max change itself at 60.0001 and is impossible to set again the correct value.

For us is a big problem.

Thanks Marco

This topic has been closed for replies.

1 reply

wired
Senior II
Sep 15, 2022 3:04 PM UTC

The Great Carnac predicts a 4.20.1 release being issued soon. X-max is being compared against Y-min instead of X-min. That could cause a lot of problems. The fact that this has been undetected until now tells me how many people are actually using the static graph (at least in the Designer).