Skip to main content
Associate II
Nov 12, 2016 2:42 PM UTC
Question

buffer size issue on ov2640

Posted on November 12, 2016 at 15:42

hi.

I drive ov2640 camera with stm32f407 by DCMI and DMA. I can get image with 160*120 resolution, so I shoud use uint16_t buff[19200] for this resolution. 

The problem is if I want to use higher resolution for example 640*480 my stm32 should have 307200*2 byte for storing the image receiving from dma to the buffer. but there is no such space in stm32f407. could you please guide me? is there any way to get the image data in a smaller part!?

#stm32f407 #ov2640 #buffer-size
This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
Nov 12, 2016 5:26 PM UTC
Posted on November 12, 2016 at 18:26

So what exactly do you want to do with data that a) takes more space than you have available, and b) comes at you quicker than you can process?

You could manage the DMA stream using a circular buffer, and managing portions of the data in the HT and TC interrupts.

If you capture the image over multiple frames it is likely to tear.

Consider using a chip with enough external memory to hold the entire frame, and has enough horsepower to process and dispatch the data at the rates desired.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
nima2Author
Associate II
Nov 14, 2016 12:07 PM UTC
Posted on November 14, 2016 at 13:07

Is there any way to use nand flash in DMA ?

Tesla DeLorean
Guru
Nov 14, 2016 5:51 PM UTC
Posted on November 14, 2016 at 18:51

NAND typically expects you to write a word and wait, and it is not fast, I don't see DMA from a synchronous source being workable.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..