Skip to main content
ksale.1
Senior II
Dec 3, 2025 10:03 PM UTC
Solved

boxProgress orientation, and circleProgress size

Hi, In my UI project I need a vertucal boxProgress while all available backgrouds and images are horizontal while w&h are greyed out. When I create a custom background, the progress bar is not working. Same for circleProgress (size control). Can you help please.

    This topic has been closed for replies.
    Osman SOYKURT
    Osman SOYKURTBest answer
    ST Technical Moderator
    Dec 5, 2025 2:03 PM UTC

    Hello @ksale.1 ,

    I attempted to replicate the issue but did not encounter any problems when setting up and using a vertical BoxProgress. Please verify the following two points:

    • Ensure that the height of your background image is sufficiently large.
    • In the properties panel of your BoxProgress widget (on the right side), adjust the "Appearance" setting—either up or down—according to your desired orientation.
      OsmanSOYKURT_1-1764943423095.png

       

     

     

    ST Software Developer | TouchGFX

    1 reply

    Osman SOYKURT
    Osman SOYKURTBest answer
    ST Technical Moderator
    Dec 5, 2025 2:03 PM UTC

    Hello @ksale.1 ,

    I attempted to replicate the issue but did not encounter any problems when setting up and using a vertical BoxProgress. Please verify the following two points:

    • Ensure that the height of your background image is sufficiently large.
    • In the properties panel of your BoxProgress widget (on the right side), adjust the "Appearance" setting—either up or down—according to your desired orientation.
      OsmanSOYKURT_1-1764943423095.png

       

     

     

    ST Software Developer | TouchGFX