Skip to main content
d.v.
Associate
Dec 18, 2019 11:41 AM UTC
Question

Blinking dots problem

Hi,

I am using TouchGFX 4.10 with STM32F769 on a custom board. My graphics includes 2 archs and 2 gauges  (added as png)  that must be rotate and two counters in the format HH:MM

When the system is active, counters must have  “:�? blinking  @2Hz and  gauges and archs must move.

To move gauges  I am using    gaugeX.updateAngles(0.0F, 0.0F, zAngle2D_x);  and to move archs i am using arcX.updateArcEnd(ARCH_END_x);

All is in the main routine  void monitorView::handleTickEvent()

No issue in moving gauges and archs…  the problem is that blinking is stopped  when archs and/or gauges are moving.

It seems that updateAngles and updateArcEnd are blocking till these routine are ended.

Any suggestion on how to solve this are welcome.

Thanks 

This topic has been closed for replies.

4 replies

Martin KJELDSEN
Principal III
Dec 19, 2019 9:02 AM UTC

Hi,

Something else is wrong. Nothing should be blocking - It works a bit different than what you think, i think. I think i'll need to see some screenshots, some code, etc.

/Martin

d.v.
d.v.Author
Associate
Dec 19, 2019 9:11 AM UTC

Hi Martin,

thanks for your answer.

I agree with you that there is something wrong in my code (it is my first TouchGFX project) and not with TouchGFX

Due to company rule, I can not share here all my code.. can I send you it in a private email? Of course when I solve the problem, I will share the solution

Thanks

Dario

Martin KJELDSEN
Principal III
Dec 19, 2019 9:16 AM UTC

I understand. How about sending it in a private message here? I'll take a look at it when i can but i'm a biiit tied up at the moment.

d.v.
d.v.Author
Associate
Dec 19, 2019 9:26 AM UTC

Hi Martin,

ok. I will prepare the files and I will write you

Many thanks

Dario