Skip to main content
Sebastian Gniazdowski
Associate III
February 3, 2017
Solved

Any description of ST Zio connection (Nucleo-144) ?

Posted on February 03, 2017 at 14:40

I have Nucleo-F767ZI board and want to use Arduino protoshield to ease making connections to a peripheral (I will solder 2x8 pin header to the shield and use a ribbon cable). However I cannot find any PDF on ST Zio connector, which will apparently be used by the Arduino shield. Where is the data?

Also, I'll be using DCMI and I'm worried that ST Zio will pin-collide with it. So it's about: which pins are used by ST Zio, particularly with Arduino shield?

Best regards,

Sebastian

#arduino #dcmi #pins #zio
This topic has been closed for replies.
Marc Laury
Marc LauryBest answer
Visitor II
February 3, 2017
Posted on February 03, 2017 at 15:03

Hi Sebastian,

you can have the description of the ST Zio connector in the following document:

http://www.st.com/content/ccc/resource/technical/document/user_manual/group0/26/49/90/2e/33/0d/4a/da/DM00244518/files/DM00244518.pdf/jcr:content/translations/en.DM00244518.pdf

I hope this can help you.

Best Regards.

Marc.

5 replies

Marc Laury
Marc LauryBest answer
Visitor II
February 3, 2017
Posted on February 03, 2017 at 15:03

Hi Sebastian,

you can have the description of the ST Zio connector in the following document:

http://www.st.com/content/ccc/resource/technical/document/user_manual/group0/26/49/90/2e/33/0d/4a/da/DM00244518/files/DM00244518.pdf/jcr:content/translations/en.DM00244518.pdf

I hope this can help you.

Best Regards.

Marc.

Amel NASRI
ST Technical Moderator
February 3, 2017
Posted on February 03, 2017 at 15:07

Hi Sebastian,

Did you checked the

http://www.st.com/content/ccc/resource/technical/document/user_manual/group0/26/49/90/2e/33/0d/4a/da/DM00244518/files/DM00244518.pdf/jcr:content/translations/en.DM00244518.pdf

(STM32 Nucleo-144 board)?

Don't you find required details there?

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
Sebastian Gniazdowski
Associate III
February 4, 2017
Posted on February 04, 2017 at 10:39

Yes the details are there, thanks. Finding this through google is hard.

Tesla DeLorean
Guru
February 4, 2017
Posted on February 04, 2017 at 16:30

>>Finding this through google is hard.

In the sense of looking in the wrong pocket for your keys kind of way...

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
MQi.1
Senior II
December 22, 2020

I have a NUCLEO-L552ZE-Q board, it was said it supports Arduino, ST Zio and morpho connectivity, and it was also said it has Arduino, Mbed and morpho connectivity. So, my question is "Is ST Zio corresponding to Mbed connectivity?"