Skip to main content
mSH.1
Associate III
Jul 20, 2022 11:26 PM UTC
Solved

An error occurs about the screen deleted from TouchGFX.

hello

​

An error occurs about the screen deleted from TouchGFX.

​

I deleted a specific screen from TouchGFX and re-generated the code.

Also, CubeIDE also deleted the Cpp file corresponding to a specific sceen.

​

Then it builds normally.

​

However, the problem is that whenever Code Generation is performed in TouhGFX, the cpps deleted in CubeIDE are recreated and an error occurs.

​

Description	Resource	Path	Location	Type
fatal error: gui_generated/scrautoremain_i4_screen/ScrAutoReMain_i4ViewBase.hpp: No such file or directory	STM32H735G-DK		line 4	C/C++ Problem
make: *** [Application/User/gui/subdir.mk:243: Application/User/gui/ScrAutoReMain_i4Presenter.o] Error 1	STM32H735G-DK		 	C/C++ Problem
make: *** [Application/User/gui/subdir.mk:245: Application/User/gui/ScrAutoReMain_i4View.o] Error 1	STM32H735G-DK		 	C/C++ Problem

​

​

Every time TouchGFX does code generation, CubeIDE is in the process of building while deleting the CPP files corresponding to the previously deleted screens one by one.

​

I want to know the solution.

​

​

thank​

​

This topic has been closed for replies.
mSH.1
mSH.1Best answer
Associate III
Jul 31, 2022 11:20 PM UTC

hello,

I found the cause.

If there is a user-added code, it occurs as above, and the user-added code must be deleted in advance.

2 replies

Yoann KLEIN
ST Employee
Jul 21, 2022 8:43 AM UTC

Hello @mSH.1​ ,

I don't understand why you are deleting manually the cpp files corresponding to the screens in CubeIDE.

If you wanna get rid of a screen, just simply delete it in TouchGFXDesigner, and then press "Refresh" on the project in STM32CubeIDE, and try to rebuild it.

The screen files and references should be deleted then.

/Yoann

Yoann KLEINST Software Developer | TouchGFX
mSH.1
mSH.1AuthorBest answer
Associate III
Jul 31, 2022 11:20 PM UTC

hello,

I found the cause.

If there is a user-added code, it occurs as above, and the user-added code must be deleted in advance.