Skip to main content
GS1
Senior III
August 5, 2020
Solved

After updating to Version 4.14.0 Image source files are differently named

Hi Martin,

I just updated my huge project from release 4.12.0 to 4.13.0 (skipped 4.13.) and generated the sources after a few minor changes.

Now Keil can not find the source files for the images anymore, because TouchGFX now placed an "image_" ahead in the file names.

I have 360 images !!! I would have to eliminate all images from the project and add the new ones in place. This is actually a time consuming job! Is there a way to get the files created as the prevois version ???

Note: I can't use the project file which is created by TouchGFX, because I have created my job long ago with one of the first versions and without CubeMX support and had to set up my project manually - you might remember this.

Thanks for any suggestions. Gaby.

This topic has been closed for replies.
Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
August 28, 2020

Hi Gaby,

We did the "image_" prefix because prefixing variables with "_" does not respect the c++ specification. (Imaging if you had an asset called main.cpp). It would generate a symbol"_main" which is protected.

/Martin

3 replies

GS1
GS1Author
Senior III
August 5, 2020

Ok, finally I've done the project file names conversion... Project working again.

Martin KJELDSEN
Martin KJELDSENBest answer
Principal III
August 28, 2020

Hi Gaby,

We did the "image_" prefix because prefixing variables with "_" does not respect the c++ specification. (Imaging if you had an asset called main.cpp). It would generate a symbol"_main" which is protected.

/Martin

GS1
GS1Author
Senior III
August 28, 2020

Ok, thanks for the info, Martin!