Skip to main content
egoltzman
Senior
January 20, 2020
Question

After porting from an older version of TouchGFX (4.9.3) to 4.13 the fonts section become huge

Hi,

I ported successfully 4.9.3 application to 4.13, the process worked well and I can see the application running under the simulation.

I tried to build the application under CubeIDE, the compilation and link passed successfully but from some reason the new version created a very large font section (More then 1M while it was around 90K)) that did not fit in the internal flash as before.

This is a short snippets from the map file of the new build:

FontFlashSection
 0x0000000091ee26b8 0x17d88c
 *(FontFlashSection FontFlashSection.*)
 FontFlashSection
 0x0000000091ee26b8 0x12f7 generated/fonts/src/Font_Poppins_Bold_16_4bpp_0.o
 0x0000000091ee26b8 unicodes_Poppins_Bold_16_4bpp_0
 *fill* 0x0000000091ee39af 0x1 
 FontFlashSection
 0x0000000091ee39b0 0x664 generated/fonts/src/Font_Poppins_Bold_16_4bpp_1.o
 0x0000000091ee39b0 unicodes_Poppins_Bold_16_4bpp_1
 FontFlashSection
 0x0000000091ee4014 0x121a9 generated/fonts/src/Font_Poppins_Bold_16_4bpp_28.o
 0x0000000091ee4014 unicodes_Poppins_Bold_16_4bpp_28

in compare to the old build:

FontFlashSection
 0x0809381c 0x16a5a
 FontFlashSection
 0x0809381c 0x130f generated/fonts/src/Font_Poppins_Bold_16_4bpp.o
 0x0809381c unicodes_Poppins_Bold_16_4bpp

Can you please explain what cause this change, and if and how I can reduce the size?

Thanks

This topic has been closed for replies.

5 replies

Martin KJELDSEN
Principal III
January 20, 2020

Hi Eyal,

Can you check the content of your generated font cpp files? Does it contain a lot more glyphs than you asked for? (Your defined ranges in the designer).

I've heard about someone else having this issue before.

/Martin

egoltzman
egoltzmanAuthor
Senior
January 20, 2020

Hi Martin,

I checked that and indeed the generated cpp are huge, I have defined ranges in the application but in the 4.9.3 version the generated cpp was much smaller so I assume (I'm not sure how to check) that in the new version I have more then I requested.

How can I fix this?

Thanks,

Eyal

egoltzman
egoltzmanAuthor
Senior
January 21, 2020

Hi Martin,

Any input on that?

Thanks

Martin KJELDSEN
Principal III
January 21, 2020

Hi Eyal,

Can you show me your unicode ranges? Can you do some experiments for me? Narrow your ranges and verify in generated code that you're getting only what you asked for - Until you don't. It's not something we've experienced yet, but i saw another user who did who solved it using a new version of his font.

But, since it works for older versions of TouchGFX there really shouldn't be a difference.

/Martin

Ggvrf.1
Visitor II
June 21, 2021

In my device I have issues with my font style the style I set there was different as compare to this one that is now showing on the screen please help me to solve this issue.