Skip to main content
TWebs.1
Associate II
February 12, 2019
Question

Advice on development kit selection for 7 or 10" display

Hello - I'm just getting started and would like to evaluate TouchGFX. I'm interested in developing for a 7 or 10" display and am trying to select an appropriate development kit. I've found these as options:

https://www.waveshare.com/product/mcu-tools/stm32/open/open746i-c-package-b.htm

Waveshare Open746-C with STM32F746IGT6 - This seems to have two display interfaces to handle both lower and higher resolution screens. Details are sketchy and I can't find what display interface is used for higher resolution screens. I don't think it supports MIPI DSI.

http://www.edtc.com/solution/ETEM070006XDH6%20Ver.2-ROHS.pdf

EDT ETEM070006XDH6 - A 7" display development kit available from EDT. Only available through the company who likely price it to find those that have an active project and are further along than I am.

https://www.st.com/en/evaluation-tools/32f769idiscovery.html

32F769IDISCOVERY - ST development kit that can come with a 4" capacitive touch display. As far as I can tell it only has the MIPI DSI interface, but can support larger displays (although I don't know enough to determine whether its RAM and external flash will support larger displays).

Since there is a TouchGFX template for the 32F769IDISCOVERY, I'm thinking that's the best choice. I could learn using the example on the 4" display, then hopefully move to a larger display when I'm ready.

Are there any options that I've missed or anything else I should consider given that I know very little about TouchGFX and my experience with displays in general is dated? My goal is to evaluate TouchGFX for use on screens 7 to 10" for use in an industrial environment.

Thanks for any advice.

This topic has been closed for replies.

3 replies

Tesla DeLorean
Guru
February 12, 2019

https://www.ghielectronics.com/products/ucm/dev-options

The RPi 7" display is on the edge of the DSI envelope. I've driven large panels with the DSI/HDMI adapter on the F769I-DISCO

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
TWebs.1
TWebs.1Author
Associate II
February 13, 2019

Thanks for the reply. What is the DSI envelope?

Tesla DeLorean
Guru
February 13, 2019

Resolution vs bandwidth vs 2 lanes.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..