Skip to main content
Associate II
Oct 29, 2024 12:44 AM UTC
Question

Administrator access for TouchGFX

Hi there Touchgfx team,

Touchgfx can not run simulator or generate code on my Win11 laptop. I found out that touchgfx needed administrator access to have those function in Win11, but Win10 not. Because my laptop is for working and provided by my company, I don't have administrator access in Win11. 

Is there any plan to fix this issue?

 

This topic has been closed for replies.

8 replies

Tesla DeLorean
Guru
Oct 29, 2024 3:31 AM UTC

>>Is there any plan to fix this issue?

If you're working on this for work, this would seem to fall squarely on your IT staff 

Perhaps you can VirtualBox a Win10 instance? Or get issued a Win10 desktop or laptop

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Associate II
Oct 29, 2024 5:12 AM UTC

Hi @Tesla DeLorean ,

Thanks for your suggestion.

I have asked for help to the IT staff. And his answer is impossible to give the administrator access to me. If touchgfx will not fix this, I have to downgrade my laptop to Win10.

ST Employee
Oct 29, 2024 12:53 PM UTC

Hello @Chand446209 ,

Could you show me what's the exact message ? 

Best regards,

Louis BOUDOST Software Engineer | TouchGFX
Associate II
Oct 30, 2024 2:45 AM UTC

Hello @LouisB ,

 

I opened a project which can generate code and run simulator with no issue in Win10. But it is failed in my Win11.

I attached two pictures for the generate code log and run simulator log. If I run touchgfx with the administrator access, both are success. 

ST Employee
Oct 31, 2024 2:09 PM UTC

Hello @Chand446209,

which version of windows 11 are you using ?

Louis BOUDOST Software Engineer | TouchGFX
ST Employee
Nov 19, 2024 2:21 PM UTC

Hello @Chand446209 ,

You are sure you have the exact same rights and configuration on the win 10 and 11 ? I looks related to your win 11 setup.

Best regards,

Louis BOUDOST Software Engineer | TouchGFX