Skip to main content
AndrewFRC135
Associate
Mar 18, 2019 10:47 PM UTC
Question

Adding STemWin to a CubeMX project without any SDRAM [Pin Conflict]

Hello Community,

I am working with a custom PCB powered by an STM32F769 that has Ethernet and LCD (no touch) hardware. The graphic requirements are quite low (320 x 240, RGB565, 150K framebuffer size), so there is no external ram on this board.

CubeMX (version 5.1.0) will not let me enable STemWin without having an SDRAM enabled in the FMC. All of the pins on the STM32F7 that can be mapped to SDCKE0, SDCKE1, SDNE0, and SDNE1 are already utilized by the ETH, LTDC, and SPI interfaces. So, I cannot simply turn on the SDRAM and point it to empty pins.

Is there a way that I can override this prerequisite to allow me to import STemWin into the project using CubeMX? If not, I assume I will need to load the STemWin files into my TrueSTUDIO project manually. It would be nice to utilize CubeMX if possible.

Thank you,

Andrew

This topic has been closed for replies.