Skip to main content
Kevin(Dr.Electron)
Associate III
August 18, 2019
Solved

Adding LwIP(or other CubeMX generated Code) to a STM32CubeIDE throws Errors in TouchGFX simulator Files.

So I started a Project in CubeIDE with the standart settings and the resolving integration issues Video.

All worked well. But now i enabled LwIP with standart Settings and I get the Error, that the SDL2/SDL_video.h File in the HALSDL2 Header couldn't be found. But shouldn't this File be excluded from the Build? How can it throw a Error in there?

Also if i restart CubeIDE and build again, sometimes i get a lot of errors in the TouchGFX/Simulator Folder, which also should be excluded.

If I disable LwIP again and restart CubeIDE it wil work again.

Versions:

CubeIDE: 1.0.1

TouchGFX: 4.10.0

MCU: STM32F746G-Discovery

Sincerly,

Kevin

This topic has been closed for replies.
Kevin(Dr.Electron)
Associate III
March 9, 2020

Sorry for the late reply, but the latest version has fixed all problems for me

6 replies

Mon2
Senior III
August 18, 2019

The toolchain is still being tweaked. Suggest for you to manually copy and past from a known good project folder what may be missing once you invoke the LwIP feature. Hoping this will allow your custom project to build correctly.

Kevin(Dr.Electron)
Associate III
August 19, 2019

That’s the Problem, if i build both Systems (LwIP and TouchGFX) separately they both work. But if i combine them, the Compiler throws errors in the exlcuded Simulator path from TouchGFX. The Compiler shouldn’t even touch this Files, because they are excluded...

Sincerely,

kevin

scottSD
Senior III
August 20, 2019

I had the same problem even when the "Exclude resource from Build" is checked. Unchecking and rechecking that selection has no effect. It is frustrating, I know. They are working on these issues and I am looking forward to a new release.

I ended up using a difference tool to compare project files from when it was working and when it wasn't and reverted some of the changes to make it compile.

The following post discusses this:

https://community.st.com/s/question/0D70X000007aSu5/cubeide-100-touchgfx-4100-working-project-inside-stm32f746gdisco?s1oid=00Db0000000YtG6&s1nid=0DB0X000000DYbd&emkind=chatterCommentNotification&emvtk=l.h0ExI045OgF3FAhHz4dq7lZP.T1nidRk255eY5dAE%3D&s1uid=0050X000008A76B&emtm=1565878208026&fromEmail=1&s1ext=0

KNg.17
Visitor II
January 13, 2020

I faced almost same error when I enable LwIP in a project with TouchGFX. After I excluded the certain files then new errors are exist. The errors are:

c:\st\stm32cubeide_1.0.2\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610\tools\bin\../lib/gcc/arm-none-eabi/7.3.1/../../../../arm-none-eabi/include/c++/7.3.1/arm-none-eabi/thumb/v7e-m/fpv4-sp/hard/bits/error_constants.h:126:31: error: 'ECANCELED' was not declared in this scope

c:\st\stm32cubeide_1.0.2\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.7-2018-q2-update.win32_1.0.0.201904181610\tools\bin\../lib/gcc/arm-none-eabi/7.3.1/../../../../arm-none-eabi/include/c++/7.3.1/arm-none-eabi/thumb/v7e-m/fpv4-sp/hard/bits/error_constants.h:135:24: error: 'EOWNERDEAD' was not declared in this scope

and etc....

Do u face this errors and have any ideas to solve it?

Dann
Visitor II
November 30, 2020

Did you find the solution? I have same errors when activate lwIP. Project was created in older version od CubeMX and TouchGFX but everything is upgraded to newest version, it didn't solve the problem.

edit: I found a solution some time ago. In my case in file:

C:\ST\STM32CubeIDE_1.6.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\include\c++\9.3.1\cerrno.h

#include <errno.h> should be changed to #include <sys/errno.h>

Kevin(Dr.Electron)
Kevin(Dr.Electron)AuthorBest answer
Associate III
March 9, 2020

Sorry for the late reply, but the latest version has fixed all problems for me