Skip to main content
Associate II
Jan 30, 2025 2:05 PM UTC
Question

Add text dynamically in Container/ScrollList

Hi, i'm kinda new to TouchGFX and i'm trying to programmatically add text inside a container of mine that i created to use as template in a ScrollList, but I was unsuccessful.

 

The idea is: For each text added, an item appears in ScrollList WITH the text

I have a textArea in touch designer with wildcard buffer

That's what im trying to do in code. At the moment, the list items appeared, but no text. Most of the code was created by ChatGPT as long as i don't know how to proceed

matheuschiarelli_0-1738245637250.png



view.cpp

#include <gui/usb_teste_screen/usb_testeView.hpp>

usb_testeView::usb_testeView() {}

void usb_testeView::setupScreen()
{
 usb_testeViewBase::setupScreen();
 addItem("Test1");
 addItem("Test2");
 addItem("Test3");
}

void usb_testeView::tearDownScreen()
{
 usb_testeViewBase::tearDownScreen();
}

void usb_testeView::addItem(const char* text)
{
 int numItems = scrollList2.getNumberOfItems();
 scrollList2.setNumberOfItems(numItems + 1); 
 scrollList2.invalidate();
}

void usb_testeView::updateItem(UsbContainer& item, int16_t itemIndex)
{
 // Convert text to Unicode::UnicodeChar
 Unicode::UnicodeChar textBuffer[256]; 
 Unicode::strncpy(textBuffer, "Teste", 256);
 textBuffer[256] = '\0'; 

 item.setText(textBuffer);
}


view.hpp

#ifndef USB_TESTE_VIEW_HPP
#define USB_TESTE_VIEW_HPP

#include <gui_generated/usb_teste_screen/usb_testeViewBase.hpp>
#include <gui/usb_teste_screen/usb_testePresenter.hpp>

class usb_testeView : public usb_testeViewBase
{
public:
 usb_testeView();
 virtual ~usb_testeView() {}
 virtual void setupScreen();
 virtual void tearDownScreen();
 void addItem(const char* text);
 void scrollWheel1UpdateItem(UsbContainer& item, int16_t itemIndex);

 void updateItem(UsbContainer& item, int16_t itemIndex);
};

#endif // USB_TESTE_VIEW_HPP


container.cpp

#include <gui/containers/UsbContainer.hpp>
#include <string.h>
#include <touchgfx/Unicode.hpp>

UsbContainer::UsbContainer()
{

}

void UsbContainer::setText(const touchgfx::Unicode::UnicodeChar* text)
{
 touchgfx::Unicode::strncpy(textArea1Buffer, text, TEXTAREA1_SIZE - 1);
 textArea1Buffer[TEXTAREA1_SIZE - 1] = '\0';

 textArea1.setWildcard(textArea1Buffer);
 textArea1.invalidate();
}

container.hpp

#ifndef USBCONTAINER_HPP
#define USBCONTAINER_HPP

#include <gui_generated/containers/UsbContainerBase.hpp>
#include <touchgfx/Unicode.hpp>


class UsbContainer : public UsbContainerBase
{
public:
 UsbContainer();
 virtual ~UsbContainer() {}

 void setText(const char* text);

 void setText(const touchgfx::Unicode::UnicodeChar* text);
};

#endif // USBCONTAINER_HPP
This topic has been closed for replies.

4 replies

ferro
Lead
Jan 30, 2025 2:55 PM UTC

Hi @matheuschiarelli 

Please share GfxDesigner project demonstating what you are trying to achieve.

Associate II
Jan 30, 2025 3:29 PM UTC

Hi, @ferro

Im trying to add items to my ScrollList via code

for example:

addItemToList("Text 1");
addItemToList("Text 2");

The final result has to be something like this:

matheuschiarelli_1-1738250211648.png

That is a ScrollList in the image.
The scrollList template is a container with an icon and a textArea with one wildcard. This is just an example of what i'm trying to achieve. Currently, "text 1" and "text 2" are not showing up.

Hope i made it clear, sorry for any inconvenience!

 

ferro
Lead
Jan 30, 2025 3:33 PM UTC

@matheuschiarelli 

I am not that familiar with ScrollList so cant help without running code sorry.

ST Employee
Feb 4, 2025 9:58 AM UTC

Hello @matheuschiarelli ,

For your issue, I will advise you to read the documentation and look at this tutorial Tutorial 4: Creating a Scroll Wheel with Custom Behavior | TouchGFX Documentation .

I hope it helps,

 

Louis BOUDOST Software Engineer | TouchGFX