Skip to main content
GMeta.1
Associate III
Aug 22, 2024 9:02 AM UTC
Solved

Add name of container for items in screen

It would be useful if an item (widget) added to a screen which is a container, showed the name of the container in the properties window. I have a lot of different containers and if I need to make changes to the container, sometimes I have to go through almost the whole list of containers to find the one I need. If the properties window in the top right of the designer window showed the name of the container, then this would be easier

Maybe also a quicker way to jump to the container either from the screens tab (context menu for example) or via the widget properties window. It is useful btw having an appropriate icon for each widget in the screens tree because you can at least tell if it is a button, line, container etc

This topic has been closed for replies.
LouisBBest answer
ST Employee
Aug 27, 2024 11:24 AM UTC

Hello @GMeta.1,

I'm not sure to understand it fully, there's already the name of the custom container in the properties :

LouisB_0-1724757958403.png

 

Best Regards,

Louis BOUDOST Software Engineer | TouchGFX

2 replies

LouisBBest answer
ST Employee
Aug 27, 2024 11:24 AM UTC

Hello @GMeta.1,

I'm not sure to understand it fully, there's already the name of the custom container in the properties :

LouisB_0-1724757958403.png

 

Best Regards,

Louis BOUDOST Software Engineer | TouchGFX
GMeta.1
GMeta.1Author
Associate III
Aug 30, 2024 7:43 AM UTC

Hi

OK maybe that was added recently. I am using version 4.19.1 and it doesn't have that:

touchgfx1.png