Skip to main content
Senior III
Oct 3, 2025 2:02 PM UTC
Question

Access modelListener and model in a singletone class

I have created a singletone class CommonUtils.cpp because I needed various functions to be used in various part of the code.

It is a very simple class like:

.cpp

#include <gui/common/CommonUtils.hpp>

CommonUtils& CommonUtils::getInstance()
{
 static CommonUtils instance;
 return instance;
}

.hpp

 

#ifndef COMMONUTILS_HPP
#define COMMONUTILS_HPP

#include <touchgfx/hal/Types.hpp>
#include <touchgfx/Unicode.hpp>
#include <gui/model/ModelListener.hpp>

class CommonUtils : public ModelListener
{
public:
 // Get singleton instance
 static CommonUtils& getInstance();
 
 // Delete copy constructor and assignment operator
 CommonUtils(const CommonUtils&) = delete;
 CommonUtils& operator=(const CommonUtils&) = delete;
private:
 // Private constructor
 CommonUtils() = default;
 ~CommonUtils() = default;

protected:
 Model* model = nullptr;
};

The class has various public function that can be call in various part of the code with 

 CommonUtils::getInstance().myFunction();

As you may have seen from the code, I have correctly linked the model to my singleton class adding the bind function and in the FrontedApplication.cpp

#include <gui/common/FrontendApplication.hpp>
#include <gui/common/CommonUtils.hpp>

FrontendApplication::FrontendApplication(Model& m, FrontendHeap& heap)
 : FrontendApplicationBase(m, heap)
{
 CommonUtils::getInstance().bindModel(&m);
}

In this why I can access the model->functionInModel 

Now, I would like to be able to access the modelListener as well on my singletone class.

Is there a way to do that?

This topic has been closed for replies.