Skip to main content
ECrom.2
Associate
Jul 10, 2022 2:20 PM UTC
Question

About touchGFX.. I installed the touchGFX not under ProgramFiles. When I cuild for target i Get a make error Can someone help solve this ? Thanks Eli

..

This topic has been closed for replies.

5 replies

MM..1
Super User
Jul 10, 2022 4:50 PM UTC

Normal place of instal isnt in ProgramFiles then your isuue must be other type. Try show error...

ECrom.2
ECrom.2Author
Associate
Jul 11, 2022 6:14 AM UTC

But I I installed in another place due to some reasons.

The Build tries to build under Programs files and generates and an error the the files are not there..

MM..1
Super User
Jul 11, 2022 4:24 PM UTC

show error

Osman SOYKURT
ST Technical Moderator
Jul 15, 2022 9:16 AM UTC

Hello ECrom.2,

TouchGFX Designer could be installed anywhere on your computer. HOWEVER you must install STM32CubeProgrammer to the default path which is "C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer" because this is where TouchGFX Designer will look for when you run on target.

/Osman

ST Software Developer | TouchGFX
ECrom.2
ECrom.2Author
Associate
Jul 17, 2022 3:29 AM UTC

Thanks

There should be a configuration param for this

Eli