Skip to main content
KKreb.1
Visitor II
Aug 17, 2020 10:27 AM UTC
Solved

X-CUBE-SBSFU - no download link yet

Hi!

I requested the download on Saturday (sorry - I missed the first mail regarding the setup and was'nt aware of the delay in granting download permission...I started the setup late on Saturday) - I read that it might take up to 48h to get the link, which would be tonight (with the actual training starting tomorrow).

Is there a way to speed up the process so I can set up the environment now to be ready for tomorrow?

    This topic has been closed for replies.
    Martin HUBIK
    Martin HUBIKBest answer
    Associate
    Aug 17, 2020 11:05 AM UTC

    Answered over Microsupport email

    2 replies

    Frantz LEFRERE
    ST Technical Moderator
    Aug 17, 2020 11:02 AM UTC

    Dear Mr Krebber,

    I sent you an email to speed up this process.

    Martin HUBIK
    Martin HUBIKBest answer
    Associate
    Aug 17, 2020 11:05 AM UTC

    Answered over Microsupport email