Skip to main content
Dhanyakumar Hosamane
Associate II
Sep 24, 2022 10:45 AM UTC
Question

X-CUBE-AWS demo project on B-L4S5I-IOT01A - Build Issue

Hi

I have downloaded en.x-cube-aws_v2-0-0.zip file. Imported STM32CubeExpansion_Cloud_AWS_V2.0.0\Projects\B-L4S5I-IOT01A\Applications\Cloud\aws_demos project in to STMCube IDE.(Version: 1.10.1)

I am able to build B-L4S5I-IOT01_2_Images_SBSFU and B-L4S5I-IOT01_2_Images_SECoreBin projects without any issues.

But the B-L4S5I-IOT01_aws_demos build fails with the following errors -

Description Resource Path Location Type

cannot use executable file '../../../../BootLoader_STSAFE/2_Images_SBSFU/STM32CubeIDE/B-L4S5I-IOT01_2_Images_SBSFU/Debug\se_interface_app.o' as input to a link B-L4S5I-IOT01_aws_demos C/C++ Problem

Is anyone facing a similar issue? any pointer to download AWS demo application for b-l4s5i-iot01a IoT eval board

Regards

Dhanya

This topic has been closed for replies.

4 replies

ST Technical Moderator
Sep 26, 2022 10:24 AM UTC

Hello @Dhanyakumar Hosamane​,

Check your setting in Properties.

Have a look at this post here: Issue building SBSFU with latest STM32CubeIDE 1.9.0 : here is the solution.

I hope this helps !

When your question is answered, please close this topic by choosing Select as Best. This will help other users find that answer faster.

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
DSahu.1
Associate
Apr 17, 2023 10:33 AM UTC

@Imen DAHMEN​  I am facing build issues with B-L4S5I-IOT01_2_Images_SECoreBin package as

 can't remove '../..\..\Inc\kms_platf_objects_config.h.tmp': No such file or directory.

Could you please specify which version of package should be considered. I am working on

https://catalog.us-east-1.prod.workshops.aws/workshops/b5857416-f2f6-4188-8562-053ec5f983ef/en-US/lab-0/lab-0-6-step-1-and-2 topic

ST Technical Moderator
Apr 17, 2023 5:12 PM UTC

Check your include path.

Go to Project options ->C/C++ tab->Include paths and add new paths to the include directories.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Associate II
Sep 5, 2023 8:10 AM UTC

Maybe we've already solved it, but,
I have experience facing a similar problem.
I recommend lowering the CUBE IDE version.
In my case, I used the 1.5.0 version and it worked out