Skip to main content
AZhar.1
Visitor II
Apr 15, 2022 2:25 PM UTC
Question

Why interrupts not occur under debug when RDP switched to level 1?

WIth oocd I try to do following steps:

1) Send reset and halt command

2) disable bit DHCSR.C_MASKINTS

3) Enable interrupts into ISER reg

4) Make any interrupt pending in ISPR reg

5) Perform Step command

if readout protection is diasabled, core interrupt occurs, I can see that pending bit is reset.

if readout protection set to 1, pending bit still set even if I will send Resume command for few seconds.

So, if there are any connection between RDP and interrupts mechanics, where can I read about it?

This topic has been closed for replies.