Skip to main content
FWguy
Associate II
Nov 1, 2021 10:26 PM UTC
Question

Where is the YMODEM code located for SBSFU?

What .c file has the code for the YMODEM portion of the SBSFU pictured below ?0693W00000GW7cAQAT.pngI have found the string "File> Transfer> YMODEM> Send" a few times, but when I changed the string to test if I found the correct area, nothing changes in the picture above.

Another tip as to why I don't think I've found the correct code location, is when I have changed the string "File> Transfer> YMODEM> Send" to say "File> Transfer> YMODEM> Send TEST" If I open the SBSFU.elf file the string is unchanged as shown below.

0693W00000GW7dXQAT.png 

This topic has been closed for replies.

9 replies

Bubbles
ST Employee
Nov 3, 2021 4:37 PM UTC

Hi @FWguy​ ,

I believe you are looking for file sfu_com_loader.c 

BR,

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
FWguy
FWguyAuthor
Associate II
Nov 3, 2021 5:02 PM UTC

Hello @JHOUD​ 

I was looking into that file too as it has a lot of the YMODEM functions, however it doesn't have the "File> Transfer> YMODEM> Send" string within that file. Maybe you see something I don't?

I'm still looking into this, but I'm now thinking it has to be changed earlier in the SBSFU pipeline. As in, maybe its code is compiled into the secure engine so I'm trying to change it to late in the process after it's been secured?

When I open the SBSFU.bin in a Hex editor and swap out the characters "File> Transfer> YMODEM> Send" to "File> Transfer> YDAVEM> Send" Then this is what gets shown after I download the file to the board and run Tera Term. So I guess another way of putting it is, I'm looking for the code that feeds into the SBSFU.bin file, what code is that and what is the YMODEM part of that code?

Bubbles
ST Employee
Nov 4, 2021 12:22 PM UTC

Hi, that could be it. You sometimes need to rebuild all three projects to be sure that a change you done is propagated into the binary.

J

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Arno1
Senior
Nov 4, 2021 10:06 AM UTC

You are looking for sfu_loader.c, line around 120.

Are you sure you are looking in the right project directory?

FWguy
FWguyAuthor
Associate II
Nov 4, 2021 4:40 PM UTC

I just took a look at sfu_loader.c around 120, and this is what I see...

I added lines 125 and 141 and added the "b" to the end of line 140. I've never seen those lines show up once I put the SBSFU.bin on the board.

0693W00000GWVGmQAP.png

Arno1
Senior
Nov 5, 2021 6:34 AM UTC

OK, lines numbers are a bit different but I wasn't looking at a clean SBSFU project.

Can you tell us which project (for which MCU/demo board) you are using and which version of x-cube-sbsfu.

You would have to use the debugger and step through the code to see where and how it reaches the line you are looking for.

FWguy
FWguyAuthor
Associate II
Nov 5, 2021 9:45 PM UTC

I've found I can change the "File> Transfer> YMODEM> Send" string in Loader_bin.o and it will show in SBSFU.elf, but now looking to see where Loader_bin.o gets compiled from. I can delete Loader_bin.o completely and it will be back once I complete compiling everything. I would think that some how the code I change in Loader.c would get compiled into Loader_Bin.o and then SBSFU.elf, but so far I haven't been able to find that link.