Skip to main content
MAlek
Associate III
Apr 17, 2019 11:22 PM UTC
Question

What is the best way to sign a message using RSA protocol ?

Hello,

what wouldd be the best library to create private/public keys (RSA) and sign some messages ?

I did not find a free library able to create and sign messages even in the smt32 crypto lib.

Any clues ?

Thank you in advance

This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
Apr 18, 2019 3:33 AM UTC
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
After Forever
Senior III
Apr 19, 2019 3:35 PM UTC

Do you really require RSA? RSA is slow and quirky, NIST recommends at least 3072 bit RSA for good security, which will be really slow on a microcontroller.

Can't you use ECC (elliptic curves) signatures? ST's crypto library provides the ED25519 algorithm which is currently one of the best available options. Alternatively, you can use ECDSA signatures (I'm not sure which curve exactly is ST using for ECDSA).

You can use a third party implementation too, for example micro-ecc for ECDSA (I recommend the secp256k1 curve) or one of many available ED25519 implementations.

MAlek
MAlekAuthor
Associate III
Apr 19, 2019 3:48 PM UTC

Yes, unfortunately, i really need RSA because it is part of a handshake where the device send me a token to be encrypted with a private RSA key.

I'e found the mbed RSA source file and it is also generated using the STM32cubeMX.

When you say RSA is slow, have you already made some tests ? How much time it will take to encrypt 1KB ?

I am just creating/organizing the environment to make some tests.

Thank you !

After Forever
Senior III
Apr 22, 2019 9:35 AM UTC

> How much time it will take to encrypt 1KB ?

It depends on your microcontroller and its running frequency, Cortex-M0 will be much slower than Cortex-M7.

Also, RSA encryption is orders of magnitude faster than decryption. For Cortex-M3/4, very approximately, expect 100-200ms for RSA-2048 encryption or signing, and 1000-2000ms for RSA-2048 decryption or verification. So, multiply it by 4 to get 1KB (2048bits / 8 = 256bytes). But generally there's no need to encrypt/decrypt more than one block of RSA data at a time, and if you are doing it - likely there's something wrong with your crypto-scheme/protocol.