Skip to main content
ADi M.507
Associate
Oct 27, 2019 5:18 PM UTC
Question

Version 2.2 bug 'mergesbsfu' bug

Hi,

Upgrading to version 2.2.0 i get this error using the option " --mergesbsfu" (Add a binary header and a sbsfu segment to an elf file):

arm-none-eabi-gcc -o "STM32F769I-Discovery_AWS.elf" @"objects.list" -mcpu=cortex-m7 -T"../STM32F769NIHx_FLASH.ld" --specs=nosys.specs -Wl,-Map="STM32F769I-Discovery_AWS.map" -Wl,--gc-sections -static -L../../../../../BootLoader_OSC/2_Images_SBSFU/SW4STM32/STM32F769I_Discovery_2_Images_SBSFU/Debug -Xlinker -L../../../../../BootLoader_OSC/Linker_Common/SW4STM32 --specs=nano.specs -mfpu=fpv5-d16 -mfloat-abi=hard -mthumb -u _printf_float -Wl,--start-group -lc -lm -Wl,--end-group
Finished building target: STM32F769I-Discovery_AWS.elf
 
arm-none-eabi-size STM32F769I-Discovery_AWS.elf 
 text	 data	 bss	 dec	 hex	filename
 248680	 13240	 242064	 503984	 7b0b0	STM32F769I-Discovery_AWS.elf
Finished building: default.size.stdout
 
arm-none-eabi-objdump -h -S STM32F769I-Discovery_AWS.elf > "STM32F769I-Discovery_AWS.list"
Finished building: STM32F769I-Discovery_AWS.list
 
arm-none-eabi-objcopy -O binary "STM32F769I-Discovery_AWS.elf" "STM32F769I-Discovery_AWS.bin"
arm-none-eabi-size "STM32F769I-Discovery_AWS.elf"
 text	 data	 bss	 dec	 hex	filename
 248680	 13240	 242064	 503984	 7b0b0	STM32F769I-Discovery_AWS.elf
"../../../../../BootLoader_OSC/2_Images_SECoreBin/SW4STM32/postbuild.sh" "../.." "./STM32F769I-Discovery_AWS.elf" "./STM32F769I-Discovery_AWS.bin" "1" "bigelf"
prepareimage with windows executeable
Generating the global elf file SBSFU and userApp
terminate called after throwing an instance of 'std::bad_alloc'
 what(): std::bad_alloc
STM32_Programmer_CLI.exe -ms ./STM32F769I-Discovery_AWS.elf ../../PostBuild/STM32F769I-Discovery_AWSsfuh.bin C:/dev/Cloud_AWS/Projects/STM32F769I-Discovery/Applications/BootLoader_OSC/2_Images_SBSFU/SW4STM32/STM32F769I_Discovery_2_Images_SBSFU/Debug/SBSFU.elf : failed
make[1]: *** [makefile:90: post-build] Error 1
make: *** [makefile:57: all] Error 2
"make all" terminated with exit code 2. Build might be incomplete.

with 2.1 it works fine..

can you fix this?

Thank you in advance, regards

Alessio DM

This topic has been closed for replies.

1 reply

alister
Senior III
Oct 27, 2019 11:18 PM UTC

I noticed it doesn't work too in the postbuild,bat version. But I didn't need the elf of the combined SBSFU and app, and just removed the 5th argument to the script in the app's post-build step.

If you need the elf, another method is convert the preceding prepareimage merge's binary out using arm-atollic-eabi-objcopy.exe.

If ST answer please explain the rationale for adding -ms to STM32_Programmer_CLI.exe.