Skip to main content
Associate II
Sep 23, 2024 3:27 PM UTC
Question

Unable to perform Regression or Debug Authentication on STM32H5

Hello,

I've been working on Provisioning my STM32H563 product and after 3 weeks of not touching the project, I am unable to perform Full Regression or Debug Authentication on my password-provisioned Nucleo Board. I tried using the generated bash scripts from CubeIDE/MX (which are using STM32_Programmer_CLI) and also STM32CubeProgrammer GUI.

I remember before the vacation, I could open and close the Board at will. I always used the same password(.bin).

Provisioning always happened using the generated provisioning.sh script.

Here is the Output of STM32CubeProgrammer (I found it has more info than dbg_auth.sh), after trying Discovery and Full Regression:

------------------------------------------------------------------

17:21:34 : Start Debug Authentication Sequence
17:21:34 : SDMOpen : 609 : open : SDM API v1.0
17:21:34 : SDMOpen : 610 : open : SDM Library version v1.1.0
17:21:34 : open_comms : 501 : open : Asserting target reset
17:21:34 : open_comms : 505 : open : Writing magic number
17:21:34 : open_comms : 515 : open : De-asserting target reset
17:21:34 : open_comms : 567 : open : Communication with the target established successfully
17:21:34 : discovery: target ID.......................:0x484
17:21:34 : discovery: SoC ID..........................:0x00000000_00000000_00000000_00000000
17:21:34 : discovery: SDA version.....................:2.4.0
17:21:34 : discovery: Vendor ID.......................:STMicroelectronics
17:21:34 : discovery: PSA lifecycle...................:ST_LIFECYCLE_CLOSED
17:21:34 : discovery: PSA auth version................:1.0
17:21:34 : discovery: ST HDPL1 status.................:0xffffffff
17:21:34 : discovery: ST HDPL2 status.................:0xffffffff
17:21:34 : discovery: ST HDPL3 status.................:0xffffffff
17:21:34 : discovery: Token Formats...................:0x200
17:21:34 : discovery: Certificate Formats.............:0x201
17:21:34 : discovery: cryptosystems...................:ST Password
17:21:34 : discovery: ST provisioning integrity status:0xeaeaeaea
17:21:34 : discovery: permission if authorized...........:Full Regression
17:21:42 : UR connection mode is defined with the HWrst reset mode
17:21:42 : Start Debug Authentication Sequence
17:21:42 : SDMOpen : 609 : open : SDM API v1.0
17:21:42 : SDMOpen : 610 : open : SDM Library version v1.1.0
17:21:42 : open_comms : 501 : open : Asserting target reset
17:21:42 : open_comms : 505 : open : Writing magic number
17:21:42 : open_comms : 515 : open : De-asserting target reset
17:21:42 : open_comms : 567 : open : Communication with the target established successfully
17:21:42 : [00%] discovery command
17:21:42 : [10%] sending discovery command
17:21:42 : [20%] receiving discovery
17:21:42 : [40%] loading credentials
17:21:42 : [50%] sending challenge request
17:21:42 : [60%] receiving challenge
17:21:42 : SDMAuthenticate : 1298 : client : Found 1 certificates
17:21:42 : [80%] sending ST password
17:21:42 : [90%] receiving response
17:21:42 : Error: Debug Authentication Failed
17:21:42 : Disconnected from device.
17:21:42 : ST-LINK SN : 0032002B3132511238363431
17:21:42 : ST-LINK FW : V3J15M6
17:21:42 : Board : NUCLEO-H563ZI
17:21:42 : Voltage : 3.25V
17:21:42 : Error: Cannot connect to access port 1! If you are trying to connect to a device with TrustZone enabled please try to connect with HotPlug mode. If you are trying to connect to a device which supports Debug Authentication with certificate or password, please open your device using it.
----------------------------------------------------------------------

What could be the issue here?

Thank you and best regards,
Stefan

This topic has been closed for replies.

2 replies

ST Employee
Sep 24, 2024 2:01 PM UTC

Hello @beartronics ,

are you sure you are selecting the same key that you used before make sure the path tp the key is correct maybe it is a naming issue.

also did you make sure that you had an application running in the non-secure world if you have TZ enabled.
make sure you check and follow the recommended steps in the related WIKI series:

Category:How to start with DA on STM32H5 - stm32mcu

Regards

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Associate II
Sep 25, 2024 1:46 PM UTC

Hello @STea ,

thank you for the reply. Sorry for duplicating this post - this one here was originally marked as spam, which is why I made another one:
https://community.st.com/t5/stm32-mcus-security/stm32h563-unable-to-regress-or-debug-authenticate

Unfortunately, your suggestions do not apply to my problem. Thanks anyways!

Best regards,
Stefan