Skip to main content
Clark Sann
Associate III
Sep 8, 2023 4:12 AM UTC
Question

Unable to import latest TFM app for B-U585I-IOTO2A using MacOS Ventura 13.5,1

I am unable to import the TFM app for the B-U585I-IOTO2A board using MacOS Ventura 13.5.1. Every time I attempt it the importer takes a long time, then fails with a 'Fail on internal error' message. I am using the Import STM32Cube Example method of importing. 

In order to fix the problem I have done the following:

1. Deleted and reinstalled STM32CubeIDE 1.13.1

2. Deleted and reinstalled the U5 library version 1.3.0

3. Rebooted the MacBook computer

These did not help at all. 

I have successfully installed the 3 required TFM projects for the STM32L562E-DK board. Those three projects installed in just a few seconds. 

It seems there is something wrong with the U5 TFM project. 

If I can provide further information, please let me know.

This topic has been closed for replies.

2 replies

Issamos
Super User
Sep 8, 2023 6:28 AM UTC

Hello @Clark Sann 

Can you retry using an older version of the U5 library. If the problem persist, try using an older version of the CubeIDE.

Best regards.

II

Clark Sann
Associate III
Sep 8, 2023 4:45 PM UTC

I can't figure out how to use an older version of the library. I deleted the latest (1.3.0) and CubeIDE forces me to download it again. I cannot find a way to import a Cube example from an older version.

I've also tried Import Existing Projects but that does not import buildable projects.

I don't think this the TFM or SBSFU projects have been tested very well for U5. L5 works great but I want to use a U5 processor.