Skip to main content
Arno1
Senior
Mar 2, 2021 8:13 AM UTC
Question

unable to complete build of project STM32H7B3I-DK

I'm trying to build the SBSFU project for board STM32H7B3I-DK (2_Images_ExtFlash) but am unable to. Everything does build fine but it fails on the last step, the postbuild.sh step, at prepareimage.py enc.

I'm using STM32CubeIDE 1.5.1 on Linux

This is the error I get:

arm-none-eabi-objcopy -O binary "UserApp.elf" "../../UserApp.bin"
arm-none-eabi-size "UserApp.elf"
 text	 data	 bss	 dec	 hex	filename
 19680	 160	 2856	 22696	 58a8	UserApp.elf
"../../../../2_Images_SECoreBin/STM32CubeIDE/postbuild.sh" "../.." "./UserApp.elf" "../../UserApp.bin" "1" "1"
prepareimage with python script
Traceback (most recent call last):
 File "STM32CubeExpansion_SBSFU_V2.4.0/Middlewares/ST/STM32_Secure_Engine/Utilities/KeysAndImages/prepareimage.py", line 861, in <module>
 args()
 File "STM32CubeExpansion_SBSFU_V2.4.0/Middlewares/ST/STM32_Secure_Engine/Utilities/KeysAndImages/prepareimage.py", line 858, in args
 subcmds[args.subcmd](args)
 File "STM32CubeExpansion_SBSFU_V2.4.0/Middlewares/ST/STM32_Secure_Engine/Utilities/KeysAndImages/prepareimage.py", line 150, in do_encrypt
 encrypted , signature , nonce_used = key.encrypt(payload, address, nonce)
 File "STM32CubeExpansion_SBSFU_V2.4.0/Middlewares/ST/STM32_Secure_Engine/Utilities/KeysAndImages/keys.py", line 102, in encrypt
 inarr = numpy.asarray(list(payload), numpy.int8).reshape(-1, 16)
 File "/usr/local/lib/python2.7/dist-packages/numpy/core/numeric.py", line 538, in asarray
 return array(a, dtype, copy=False, order=order)
ValueError: invalid literal for long() with base 10: ''
python STM32CubeExpansion_SBSFU_V2.4.0/Middlewares/ST/STM32_Secure_Engine/Utilities/KeysAndImages/prepareimage.py enc -k ../../../../2_Images_SECoreBin/STM32CubeIDE/../Binary/OEM_KEY_COMPANY1_key_AES_CTR.bin -n ../../../../2_Images_SECoreBin/STM32CubeIDE/../Binary/nonce.bin -a 0x09000040 ../../UserApp.bin ../../../Binary/UserApp.sfu : failed
make[1]: *** [makefile:90: post-build] Error 1
make: *** [makefile:56: all] Error 2
"make all" terminated with exit code 2. Build might be incomplete.

(some paths truncated)

There is no nonce.bin in Projects/STM32H7B3I-DK/Applications/2_Images_ExtFlash/2_Images_SECoreBin/Binary but after adding the one from 2_Images (without ExtFlash) I get the same error.

Best regards,

Arno

This topic has been closed for replies.

1 reply

Jocelyn RICARD
ST Employee
Mar 12, 2021 10:31 AM UTC

Hello Arno,

I tried to reproduce the issue on a Ubuntu 16.04 LTS with same version of STM32CubeIDE.

I could see 2 issued while building the loader:

1- Need to change '\' by '/' in the ld file path in the properties

2- Need to activate the VFP also in properties

After that all when well until UserApp build.

One possible reason for your issue is the too long path where the package is installed.

Best regards

Jocelyn