Skip to main content
Eugene G
Associate II
Mar 23, 2021 3:48 AM UTC
Question

Unable to build the any SBSFU projects

I'm following the security part 6 - 02 Building the SBSFU but the final build of the UserApp always ends up with an error.

Instructions are being followed EXACTLY as in the video. I'm getting a different project size when building the SBSFU, slightly larger at 59874 instead of 59578 as mentioned in the video and the documentation. Going on to the next step of building the UserApp will always fail with this error:

c:\st\stm32cubeide_1.0.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: ../../../../../../../../Projects/NUCLEO-L476RG/Applications/2_Images/2_Images_SBSFU/SW4STM32/STM32L476RG_NUCLEO_2_Images_SBSFU/Debug\se_interface_app.o: in function `SE_APP_GetActiveFwInfo':

(.SE_IF_Code+0x0): multiple definition of `SE_APP_GetActiveFwInfo'; ../../../../../../../../Projects/NUCLEO-L476RG/Applications/2_Images/2_Images_SBSFU/SW4STM32/STM32L476RG_NUCLEO_2_Images_SBSFU/Debug\se_interface_app.o:(.SE_IF_Code+0x0): first defined here

I'm running CubeIDE 1.6 and cube programmer 2.7 (tried with 2.5 as well). Will I need to downgrade Cube IDE as well?

    This topic has been closed for replies.

    2 replies

    Frantz LEFRERE
    ST Technical Moderator
    Mar 23, 2021 6:50 AM UTC

    Infact this is a regression with CubeIDE 1.6.0.

    Workaround has been describe by my colleague Jocelyn here :

    https://community.st.com/s/question/0D53W00000cRsLA/the-update-to-cubeide-160-cause-a-linker-error-compiling-the-userapp

    Sump up of the workaround :

    1) Removing the -l:se_interface_app.o from Tools Settings/Libraries/Libraries

    2) Adding the same -l:se_interface_app.o in Tool Settings/Miscellaneous/Other flags

    Eugene G
    Eugene GAuthor
    Associate II
    Mar 23, 2021 8:00 AM UTC

    That fixed it. Thanks!