Skip to main content
PDres.1
Visitor II
Mar 3, 2021 6:33 PM UTC
Solved

The update to CubeIDE 1.6.0 cause a linker error compiling the UserApp.

(.SE_IF_Code+0x0): multiple definition of `SE_APP_GetActiveFwInfo'

STM32L476 Demo

This topic has been closed for replies.
Jocelyn RICARD
Jocelyn RICARDBest answer
ST Employee
Mar 5, 2021 6:13 PM UTC

Hello,

I confirm the issue. And looking into the command line, the -l:se_interface_app.o is added twice.

I could make the compilation work by

1) Removing the -l:se_interface_app.o from Tools Settings/Libraries/Libraries

2) Adding the same -l:se_interface_app.o in Tool Settings/Miscellaneous/Other flags

Best regards

Jocelyn

6 replies

ST Technical Moderator
Mar 4, 2021 8:13 AM UTC

Hello @Community member​ and welcome to the STM32 Community :smiling_face_with_smiling_eyes:

I added the topic "STM32CubeIDE" to your question to be reviewed by our CubeIDE experts.

Hi @Markus GIRDLAND​ ,

Can you please help @Community member​ on this issue?

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Fred
ST Employee
Mar 4, 2021 9:07 AM UTC

As a workaround, you should be able to compile properly by placing the se_interface_app.o object file in the "Linker => Miscellaneous => Additional object flags" instead if the "Linker => Libraries => Libraries" (in the UserApp project).

Jocelyn RICARD
Jocelyn RICARDBest answer
ST Employee
Mar 5, 2021 6:13 PM UTC

Hello,

I confirm the issue. And looking into the command line, the -l:se_interface_app.o is added twice.

I could make the compilation work by

1) Removing the -l:se_interface_app.o from Tools Settings/Libraries/Libraries

2) Adding the same -l:se_interface_app.o in Tool Settings/Miscellaneous/Other flags

Best regards

Jocelyn

GMate.11
Associate
Apr 21, 2021 4:56 AM UTC

Hi Jocelyn,

i habe in deep the same problem

c:\st\stm32cubeide_1.2.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: ../Core/Inc/new_main.h:16: multiple definition of `huart_MHZ19C'; ../Core/Inc/new_main.h:16: first defined here...

But in my case, there is nothing to delete on Libraries

0693W00000AM3UhQAL.pngI added the object on the micellaneous and compile agin

0693W00000AM3VLQA1.pngEventhough the changes. i get the same error

I appreciate your comments

STM32Fan1
Visitor II
Mar 25, 2021 4:05 PM UTC

Hi,

it works thanks Jocelyn

Just adding some infos where I found these options

click right when selecting the project which fail linking

Then properties

Got to C/C++ build setting

MCU GCC linker in Librairies you have entry :se_interface_app.o

remove it but select & clicking on the red cross icon

then select MCU GCC Linker/Miscellaneous

add -l:se_interface_app.o (please note the -l before)

Wait a bit for build and enjoy

Problem is solved

Vincent

Amin.TAYEBI
Associate II
Jul 7, 2021 1:24 PM UTC

Hi

I solved the problem by disconnecting and connecting the stm32-wl55c1 from my PC while pressing Debug botton in Cube-IDE.

Amin TAYEBI