Skip to main content
Visitor II
November 13, 2025
Question

STMU575ZI-Q TFM Port attempt: DEV TARGET NOT HALTED / The interface firmware FAILED to reset/halt the target MCU

Hi everyone, I was trying to port TFM + TFM_SB on my STMU575ZI-Q Nucleo following this guide: https://www.st.com/resource/en/user_manual/um2851-getting-started-with-stm32cubeu5-tfm-application-stmicroelectronics.pdf and I've managed to flash secure bootloader and TFM. I've managed to do the regression of the MCU setting the option bytes. When I finally lunched TFM_UPDATE.sh script, logs appeared on tera term as expected, but in the end it got stuck in TFM BOOT log. So I disconnected the board and tried to repeat the process, cleaning and building again the TFM SB image, TFM Appl image etc... But When I tried to mass erase the system flash, an error has occurred: DEV TARGET NOT HALTED. When I reset the board and I observe tera term logs, I can see the following:

[INF] Flash operation: Op=0x0, Area=0x0, Address=0x0

[INF] Starting bootloader

[INF] Checking BL2 NV area

[INF] Checking BL2 NV area header

[INF] Checking BL2 NV Counter consistency

[INF] Consistent BL2 NV Counter 3 = 0x1000000

[INF] Consistent BL2 NV Counter 4 = 0x1000000

[INF] Consistent BL2 NV Counter 5 = 0x1000000

[INF] Consistent BL2 NV Counter 6 = 0x1000000

[INF] Swap type: none

[INF] Swap type: none

[INF] Swap type: none

[INF] Swap type: none

[INF] verify counter 0 1000000 1000000

[INF] counter 0 : ok

[INF] hash ref OK

[INF] verify counter 1 1000000 1000000

[INF] counter 1 : ok

[INF] hash ref OK

[INF] verify counter 2 1000000 1000000

[INF] counter 2 : ok

[INF] hash ref OK

[INF] verify counter 3 1000000 1000000

[INF] counter 3 : ok

[INF] hash ref OK

[INF] Bootloader chainload address offset: 0x28000

[INF] Jumping to the first image slot

[INF] BL2 HUK 5f5f5f5f5f4b5548..5f45554c5f5f5f5f set to BL2 SHARED DATA

[INF] BL2 SEED fc0f9140ca3243b1..dd711a1f156ad759 set to BL2 SHARED DATA

[INF] Code c006000 c0184f8

[INF] hash TFM_SBSFU_Boot 5e49fe67 .. 155df3f1


It could be due to a bad port? I would like to understand the exact reason why it happened. When I connect the board via USB, I can see the following error printed in a txt file:

The interface firmware FAILED to reset/halt the target MCU

I tried different things to solve this error and manage to gain back the connection to the board, including:

Trying to connect under reset, switching reset mode, frequency on stmcubeprogrammer, trying to use stm cube programmer CLI, trying to connect PIN 5 and 7 to force boot0 to high (which, if I correctly understood, should force the board to boot with the system bootloader), but nothing seems to work.

 

1 reply

Jocelyn RICARD
ST Employee
December 3, 2025

Hello @wxman9 ,

if you check Table 9, by default RDP Level 1 is enabled, but BOOTçLOCK is not enabled.

This means that if you connect BOOT0 to VDD you should be able to attach in hotplug mode, or connect with USB and request a regression.

Then you should change boot_hal_cfg.h file to leave the board in RDP Level 0 after provisioning, allowing you to debug.

One remark. TFM is no more supported inside STM32CubeU5. First reason is that TFM version was 1.3 which is from 2021... 

You can still have TFM on STM32U5 but through trusted_firmware.org. You will need to build with cmake/ninja.

Best regards

Jocelyn