Skip to main content
Associate II
Feb 21, 2025 9:11 AM UTC
Question

STM32WLxx DFU Error

Hi,

I ported the SBSFU project to the LoRaWAN_AT_Slave routine, and tested DFU normally and it worked fine, but when I used the wrong file to upgrade, such as readme.txt, the upgrade process ran for a while, and then stopped, showed " Fw header authentication error" and "No valid FW found in the active slots nor new FW to be installed". As a result, the firmware of my application cannot run normally, and I must re-DFU the normal firmware before I can restore it. Is this normal?

ethan2_0-1740128888124.png

 

This topic has been closed for replies.

3 replies

STTwo-32
ST Technical Moderator
Feb 21, 2025 10:24 AM UTC

Hello @ethan2 

Please add more details on your configurations what steps have you been following, what is the readme you are toking about, what is the "Wrong file"...

Best Regards.

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ethan2Author
Associate II
Feb 24, 2025 2:22 AM UTC

Hi STTwo-32,

I refer to < UM2767-geting-start-with-the-SBsfu-of-STM32Cubewl-stmicroelectronics > for the upgrade. The error readme.txt simply means that I did not use the generated xx.sfb file, but imported a txt file.