Skip to main content
Lbour.1
Associate
June 29, 2021
Solved

STM32WLE5 write locked not in read after passing RDP from Level 1 to Level 0

Hello,

I use STM32WLE5 on a seed studio module LORA-E5 mini where boot0 is not accessible (completely crazy ...). The module comes with a read protection and they ask us to remove RDP (level 1 to level 0) to be able to flash it with a custom program.

I was able to pass RDP from 0xBB to 0xAA in hotplug mode, all was ok exept that I cannot now erase or flash anything. I can connect in normal mode at any speed, read option bytes but no flashing. Sometimes I can erase one page but it is random ?

V target is 3.16V

stlink v2 firmware : V3j37S7

Masse erase output :

 10:15:43:555 : MASS ERASE ...

 10:15:43:555 : Flash erase...

 10:15:43:558 : halt ap 0

 10:15:43:558 : w ap 0 reg 15 PC  (0x20000000) 

 10:15:43:559 : w ap 0 reg 17 MSP (0x20000500) 

 10:15:43:561 : w ap 0 reg 16 xPSR (0x01000000) 

 10:15:43:568 : w ap 0 @0x20001380 0x00000200 bytes Data 0x00000000

 10:15:43:568 : w ap 0 @0x20000000 0x00000004 bytes Data 0x0000BE00

 10:15:43:607 : w ap 0 @0x20000004 0x00000F54 bytes Data 0x0001B510

 10:15:43:607 : Init flashloader...

 10:15:43:609 : halt ap 0

 10:15:43:610 : w ap 0 reg 0 R0  0x00000001

 10:15:43:610 : w ap 0 reg 1 R1  0x00000000

 10:15:43:610 : Loader mass erase...

 10:15:43:610 : Error: Mass erase operation failed.Please verify flash protection

Page erase output :

10:16:50:708 : Flash sector erase ...

 10:16:50:710 : Flash erase...

 10:16:50:712 : halt ap 0

 10:16:50:712 : w ap 0 reg 15 PC  (0x20000000) 

 10:16:50:713 : w ap 0 reg 17 MSP (0x20000500) 

 10:16:50:714 : w ap 0 reg 16 xPSR (0x01000000) 

 10:16:50:724 : w ap 0 @0x20001380 0x00000200 bytes Data 0x00000000

 10:16:50:724 : w ap 0 @0x20000000 0x00000004 bytes Data 0x0000BE00

 10:16:50:763 : w ap 0 @0x20000004 0x00000F54 bytes Data 0x0001B510

 10:16:50:764 : Init flashloader...

 10:16:50:766 : halt ap 0

 10:16:50:767 : w ap 0 reg 0 R0  0x00000001

 10:16:50:768 : w ap 0 reg 1 R1  0x00000000

 10:16:50:769 : w ap 0 reg 2 R2  0x00000000

 10:16:50:769 : w ap 0 reg 3 R3  0x00000000

 10:16:50:770 : w ap 0 reg 4 R4  0x00000000

 10:16:50:772 : w ap 0 reg 5 R5  0x00000000

 10:16:50:773 : w ap 0 reg 6 R6  0x00000000

 10:16:50:774 : w ap 0 reg 7 R7  0x00000000

 10:16:50:774 : w ap 0 reg 8 R8  0x00000000

 10:16:50:774 : w ap 0 reg 9 R9  0x00000000

 10:16:50:774 : w ap 0 reg 10 R10 0x00000000

 10:16:50:775 : w ap 0 reg 11 R11 0x00000000

 10:16:50:776 : w ap 0 reg 12 R12 0x00000000

 10:16:50:776 : w ap 0 reg 13 SP  0x00000000

 10:16:50:777 : w ap 0 reg 14 LR  0x20000001

 10:16:50:778 : w ap 0 reg 15 PC  0x2000002F

 10:16:50:779 : w ap 0 reg 16 xPSR 0x01000000

 10:16:50:780 : w ap 0 reg 17 MSP 0x20001354

 10:16:50:780 : w ap 0 reg 18 PSP 0x00000000

 10:16:50:780 : run ap 0

 10:16:50:780 : halt ap 0

 10:16:50:781 : r ap 0 reg 0 R0  0x00000001

 10:16:50:781 : Loader sector erase...

 10:16:50:784 : w ap 0 reg 0 R0  0x08000000

 10:16:50:785 : w ap 0 reg 1 R1  0x08000000

 10:16:50:785 : w ap 0 reg 2 R2  0x00000002

 10:16:50:786 : w ap 0 reg 3 R3  0x00000000

 10:16:50:786 : w ap 0 reg 4 R4  0x00000000

 10:16:50:786 : Error: Sector erase operation has failed at least for one of the existing specified sectors.Please verify flash memory protection.

Thanks for your help.

Laurent

This topic has been closed for replies.
Lbour.1
Lbour.1Best answer
Associate
June 30, 2021

I solved the problem :

RDB was locked at 0xAA and still no erase or flash capability, you need to set again RDP to 0xBB , unplug the board (very important, if not it will not work and stay locked at 0xAA), reconnect to the stm32, you will see RDP with a strange value 0xFF, that is ok, and set back RDP to 0xAA, this time you will be able to change the value.

Today all is ok, I can erase and flash anything :) very very very strange .....

2 replies

Lbour.1
Lbour.1AuthorBest answer
Associate
June 30, 2021

I solved the problem :

RDB was locked at 0xAA and still no erase or flash capability, you need to set again RDP to 0xBB , unplug the board (very important, if not it will not work and stay locked at 0xAA), reconnect to the stm32, you will see RDP with a strange value 0xFF, that is ok, and set back RDP to 0xAA, this time you will be able to change the value.

Today all is ok, I can erase and flash anything :) very very very strange .....

EP.2
Associate II
December 17, 2023

Thanks very much, I had the same issue, couldn't read or write the device even though RDP 0xAA. I couldn't even change any of the user bytes or Option bytes. So I set RDP to 0xBB, power cycled, it showed as 0xFF, then I set it back to 0xAA and then everything went back to normal. I had to reset all the user bytes back to default, but other than that it seems OK.