Skip to main content
Associate II
Aug 29, 2025 1:21 PM UTC
Question

STM32U585 TrustZone ADC DMA-buffer always 0

Hi, I'm using 3 channels of ADC4 with GPDMA1 (channel 4) in secure world of a TrustZone-project and the DMA-buffer stays always 0. The same ADC/DMA-configuration with the same application code (all mnus the security aspects) are working fine without TrustZone on the same hardware. I set the DMA-channel and the ADC-channel to secure and privileged, also the SAU-configuration for these peripherals is secure, the DMA-interrupt (circular) is triggered and calling HAL_ADC_ConvCpltCallback but there's nothing inside the DMA-buffer (which is defined as volatile inside a secure and privileged SRAM-area). I've tried different ADC conversion rates, clock rates and clock sources, checked for errors (especially overruns) and secure faults (with GTZC), there's absolutely nothing. I guess it must have something to do with secure/privileged areas or peripherals but since all the parts are secure and privileged I don't know what it could be. I'd be thankful for any suggestions; here is my ADC DMA-initialization code:

void MX_ADC4_Init(void)
{

 /* USER CODE BEGIN ADC4_Init 0 */

 /* USER CODE END ADC4_Init 0 */

 ADC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN ADC4_Init 1 */

 /* USER CODE END ADC4_Init 1 */

 /** Common config
 */
 hadc4.Instance = ADC4;
 hadc4.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV64;
 hadc4.Init.Resolution = ADC_RESOLUTION_12B;
 hadc4.Init.DataAlign = ADC_DATAALIGN_RIGHT;
 hadc4.Init.ScanConvMode = ADC4_SCAN_ENABLE;
 hadc4.Init.EOCSelection = ADC_EOC_SEQ_CONV;
 hadc4.Init.LowPowerAutoPowerOff = ADC_LOW_POWER_NONE;
 hadc4.Init.LowPowerAutoWait = DISABLE;
 hadc4.Init.ContinuousConvMode = ENABLE;
 hadc4.Init.NbrOfConversion = 3;
 hadc4.Init.ExternalTrigConv = ADC_SOFTWARE_START;
 hadc4.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE;
 hadc4.Init.DMAContinuousRequests = ENABLE;
 hadc4.Init.TriggerFrequencyMode = ADC_TRIGGER_FREQ_HIGH;
 hadc4.Init.Overrun = ADC_OVR_DATA_OVERWRITTEN;
 hadc4.Init.SamplingTimeCommon1 = ADC4_SAMPLETIME_7CYCLES_5;
 hadc4.Init.SamplingTimeCommon2 = ADC4_SAMPLETIME_1CYCLE_5;
 hadc4.Init.OversamplingMode = ENABLE;
 hadc4.Init.Oversampling.Ratio = ADC_OVERSAMPLING_RATIO_2;
 hadc4.Init.Oversampling.RightBitShift = ADC_RIGHTBITSHIFT_1;
 hadc4.Init.Oversampling.TriggeredMode = ADC_TRIGGEREDMODE_SINGLE_TRIGGER;
 if (HAL_ADC_Init(&hadc4) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_9;
 sConfig.Rank = ADC4_REGULAR_RANK_1;
 sConfig.SamplingTime = ADC4_SAMPLINGTIME_COMMON_1;
 sConfig.OffsetNumber = ADC_OFFSET_NONE;
 sConfig.Offset = 0;
 if (HAL_ADC_ConfigChannel(&hadc4, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_10;
 sConfig.Rank = ADC4_REGULAR_RANK_2;
 if (HAL_ADC_ConfigChannel(&hadc4, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }

 /** Configure Regular Channel
 */
 sConfig.Channel = ADC_CHANNEL_11;
 sConfig.Rank = ADC4_REGULAR_RANK_3;
 if (HAL_ADC_ConfigChannel(&hadc4, &sConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN ADC4_Init 2 */

 /* USER CODE END ADC4_Init 2 */

}

void HAL_ADC_MspInit(ADC_HandleTypeDef* adcHandle)
{

 GPIO_InitTypeDef GPIO_InitStruct = {0};
 DMA_NodeConfTypeDef NodeConfig= {0};
 RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
 if(adcHandle->Instance==ADC4)
 {
 /* USER CODE BEGIN ADC4_MspInit 0 */

 /* USER CODE END ADC4_MspInit 0 */

 /** Initializes the peripherals clock
 */
 PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_ADCDAC;
 PeriphClkInit.AdcDacClockSelection = RCC_ADCDACCLKSOURCE_HCLK;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
 {
 Error_Handler();
 }

 /* ADC4 clock enable */
 __HAL_RCC_ADC4_CLK_ENABLE();

 __HAL_RCC_GPIOA_CLK_ENABLE();
 /**ADC4 GPIO Configuration
 PA4 ------> ADC4_IN9
 PA5 ------> ADC4_IN10
 PA6 ------> ADC4_IN11
 */
 GPIO_InitStruct.Pin = GPIO_PIN_4|GPIO_PIN_5|GPIO_PIN_6;
 GPIO_InitStruct.Mode = GPIO_MODE_ANALOG;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /* ADC4 DMA Init */
 /* GPDMA1_REQUEST_ADC4 Init */
 NodeConfig.NodeType = DMA_GPDMA_LINEAR_NODE;
 NodeConfig.SrcSecure = DMA_CHANNEL_SRC_SEC;
 NodeConfig.DestSecure = DMA_CHANNEL_DEST_SEC;
 NodeConfig.Init.Request = GPDMA1_REQUEST_ADC4;
 NodeConfig.Init.BlkHWRequest = DMA_BREQ_SINGLE_BURST;
 NodeConfig.Init.Direction = DMA_PERIPH_TO_MEMORY;
 NodeConfig.Init.SrcInc = DMA_SINC_FIXED;
 NodeConfig.Init.DestInc = DMA_DINC_INCREMENTED;
 NodeConfig.Init.SrcDataWidth = DMA_SRC_DATAWIDTH_HALFWORD;
 NodeConfig.Init.DestDataWidth = DMA_DEST_DATAWIDTH_HALFWORD;
 NodeConfig.Init.SrcBurstLength = 1;
 NodeConfig.Init.DestBurstLength = 1;
 NodeConfig.Init.TransferAllocatedPort = DMA_SRC_ALLOCATED_PORT0|DMA_DEST_ALLOCATED_PORT0;
 NodeConfig.Init.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER;
 NodeConfig.Init.Mode = DMA_NORMAL;
 NodeConfig.TriggerConfig.TriggerPolarity = DMA_TRIG_POLARITY_MASKED;
 NodeConfig.DataHandlingConfig.DataExchange = DMA_EXCHANGE_NONE;
 NodeConfig.DataHandlingConfig.DataAlignment = DMA_DATA_RIGHTALIGN_ZEROPADDED;
 NodeConfig.SrcSecure = DMA_CHANNEL_SRC_SEC;
 NodeConfig.DestSecure = DMA_CHANNEL_DEST_SEC;
 if (HAL_DMAEx_List_BuildNode(&NodeConfig, &Node_GPDMA1_Channel4) != HAL_OK)
 {
 Error_Handler();
 }

 if (HAL_DMAEx_List_InsertNode(&List_GPDMA1_Channel4, NULL, &Node_GPDMA1_Channel4) != HAL_OK)
 {
 Error_Handler();
 }

 if (HAL_DMAEx_List_SetCircularMode(&List_GPDMA1_Channel4) != HAL_OK)
 {
 Error_Handler();
 }

 handle_GPDMA1_Channel4.Instance = GPDMA1_Channel4;
 handle_GPDMA1_Channel4.InitLinkedList.Priority = DMA_LOW_PRIORITY_LOW_WEIGHT;
 handle_GPDMA1_Channel4.InitLinkedList.LinkStepMode = DMA_LSM_FULL_EXECUTION;
 handle_GPDMA1_Channel4.InitLinkedList.LinkAllocatedPort = DMA_LINK_ALLOCATED_PORT0;
 handle_GPDMA1_Channel4.InitLinkedList.TransferEventMode = DMA_TCEM_BLOCK_TRANSFER;
 handle_GPDMA1_Channel4.InitLinkedList.LinkedListMode = DMA_LINKEDLIST_CIRCULAR;
 if (HAL_DMAEx_List_Init(&handle_GPDMA1_Channel4) != HAL_OK)
 {
 Error_Handler();
 }

 if (HAL_DMAEx_List_LinkQ(&handle_GPDMA1_Channel4, &List_GPDMA1_Channel4) != HAL_OK)
 {
 Error_Handler();
 }

 __HAL_LINKDMA(adcHandle, DMA_Handle, handle_GPDMA1_Channel4);

 if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel4, DMA_CHANNEL_PRIV|DMA_CHANNEL_SEC) != HAL_OK)
 {
 Error_Handler();
 }

 /* ADC4 interrupt Init */
 HAL_NVIC_SetPriority(ADC4_IRQn, 5, 0);
 HAL_NVIC_EnableIRQ(ADC4_IRQn);
 /* USER CODE BEGIN ADC4_MspInit 1 */

 /* USER CODE END ADC4_MspInit 1 */
 }
}
void MX_GPDMA1_Init(void)
{
 /* Peripheral clock enable */
 __HAL_RCC_GPDMA1_CLK_ENABLE();

 /* GPDMA1 interrupt Init */
 HAL_NVIC_SetPriority(GPDMA1_Channel4_IRQn, 4, 0);
 HAL_NVIC_EnableIRQ(GPDMA1_Channel4_IRQn);
}
This topic has been closed for replies.

3 replies

Jocelyn RICARD
ST Employee
Oct 8, 2025 9:43 PM UTC

Hello @AAArdvark ,

the GPDMA is unsecure by default.

You can see GPDMA_SECCFGR that defaults 0, meaning all channels are unsecure.

Same for GPDMA_PRIVCFGR that default value is 0 meaning all channels are unprivileged.

In your code I can see that channels are set secure but privileged is not set. This is probably the reason it fails

Best regards

Jocelyn

AAArdvarkAuthor
Associate II
Oct 9, 2025 9:51 AM UTC

Hello Jocelyn,

Thank you for your answer; in the code I posted there are these lines:

 if (HAL_DMA_ConfigChannelAttributes(&handle_GPDMA1_Channel4, DMA_CHANNEL_PRIV|DMA_CHANNEL_SEC) != HAL_OK)
 {
 Error_Handler();
 }

I guess that should set the DMA-channel to secure as well as privileged or am I overseeing something?

Best regards 

Jocelyn RICARD
ST Employee
Oct 9, 2025 5:51 PM UTC

Hello @AAArdvark ,

yes my bad, I missed that.

You say in your post that you set everything secure. So, you confirm that ADC and SRAM are both secure/privilege and GPIOs are also secure ?

I guess you are also using secure alias for buffer address.

Last point, did you enable cache ? But as you say it is working in non secure, this is unlikely the issue.

I would need to reproduce this issue to try finding what happens.

If you can share a code, this would help

Best regards

Jocelyn