Skip to main content
OliM
Senior II
May 6, 2026
Solved

STM32U585: Start bootloader via RSS command

I have a STM32U585 (edit: ...VIT6, so not the one where this doesn't work due to errata) product with Trustzone enabled, Bootlock disabled and RDP level 0.
I want to bring this into ST bootloader mode from software (for easy Firmware change via USB).

To my understanding that would mean implementing the last entry of Pattern 12 from AN2606

OliM_1-1778070843232.png

 

OliM_0-1778070786976.png

 

Which means the following code, executed from secure side.

RCC->APB3ENR |= RCC_APB3ENR_SYSCFGEN; //clock is disabled after startup, so enable
__DSB();//make sure data is written
SYSCFG->RSSCMDR = 0x1C0; //pattern from AN2606, RM says any value will do? 
__DSB();//make sure data is written
__NVIC_SystemReset(); //SW reset

 But all I get is a restart to SECBOOTADD0. And RSSCMDR is zeroed out afterwards, even though the RM states that it is only affected by power on reset.

What am I doing wrong?

OliM
OliMBest answer
Senior II
June 17, 2026

Through a support ticket I got the info that actually RSS Commands 0x01 and 0x02 have the desired effect.

2 replies

OliM
OliMAuthor
Senior II
May 20, 2026

Noone ever did this?

OliM
OliMAuthorBest answer
Senior II
June 17, 2026

Through a support ticket I got the info that actually RSS Commands 0x01 and 0x02 have the desired effect.