STM32U5 SBSFU: "[WRN] 15 status write fails performing the swap" using custom flash layout
- 1 reply
- 253 views
Hi everyone,
I am working on a custom board based on the STM32U575RGT6 (TrustZone enabled, FreeRTOS). I have successfully ported the SBSFU example originally provided for the B-U585I-IOT02A.
My configuration is:
- MCUBOOT_APP_IMAGE_NUMBER = 1 (Single combined S and NS image)
- No external loader.
To meet my application needs, I added a custom FLASH_STORAGE area at the end of the flash for EEPROM emulation. To do this cleanly, I modified flash_layout.h to dynamically compute the available FLASH_NS_PARTITION_SIZE based on the remaining space.
The Problem: When I use MCUBOOT_OVERWRITE_ONLY, the OTA update (via Y-Modem) works perfectly. However, when I try to use the Swap mode (by commenting out #define MCUBOOT_OVERWRITE_ONLY), the firmware download succeeds, the board reboots, the bootloader validates the signature, starts the swap process, but then crashes with a status write fail:
FWUPDATE
--- Démarrage de la mise à jour Firmware (Non-Secure) ---
-- Erasing download area
-- Send Firmware
-- -- File> Transfer> YMODEM> Send
I/commMonitoring [356203] Demande de mise à jour Firmware reçue !
.e_result = 0 , 3
-- -- Programming Completed Successfully!
-- -- Bytes: 264392
Write Magic Trailer at edff0
-- Firmware téléchargé avec succès ! Redémarrage imminent...
[INF] Flash operation: Op=0x0, Area=0x0, Address=0x0
[INF] Starting bootloader OEMiROT
[INF] Checking BL2 NV area
[INF] Checking BL2 NV area header
[INF] Checking BL2 NV Counter consistency
[INF] Consistent BL2 NV Counter 0 = 0x1000000
[INF] Primary image: magic=good, swap_type=0x1, copy_done=0x3, image_ok=0x1
[INF] Scratch: magic=unset, swap_type=0x1, copy_done=0x3, image_ok=0x3
[INF] Boot source: primary slot
[INF] Swap type: test
[INF] ce, e2, 8e, fc, e0, 8c , 73 ,e9,
[INF] 6d, f7, 78, 68, 56, 52 , 3e ,1f,
[INF] verify counter 0 1000000 1000000
[INF] counter 0 : ok
[INF] verify sig key id 0
[INF] checking public key 47 5b
[INF] verifying signature hlen 20
[INF] signature OK
[INF] a2, 33, da, b4, 77, a0 , ef ,ee,
[INF] 78, 6f, 70, db, c0, de , c3 ,7a,
[INF] Swapping secondary and primary slots: 0x408c8 bytes
[INF] Swapping: swap index 0x0, sector index 0x19, size 0x10000
[INF] Swapping: swap index 0x1, sector index 0x11, size 0x10000
[INF] Swapping: swap index 0x2, sector index 0x9, size 0x10000
[INF] Swapping: swap index 0x3, sector index 0x1, size 0x10000
[INF] Swapping: swap index 0x4, sector index 0x0, size 0x2000
[WRN] 15 status write fails performing the swap
[ERR] panic!What I suspect: Since OVERWRITE works fine, I suspect that resizing the partitions and using the SCRATCH area breaks a hardcoded security rule in SBSFU_Boot (possibly in low_level_device.c with write_vect/secure_vect, or in the SAU/MPU config inside low_level_security.c). I noticed that the single image trailer is physically located in the Non-Secure flash space, which might be rejected during the swap status write.
Here is the relevant part of my custom flash_layout.h showing the dynamic size calculation:
/* 1. USER CUSTOM CONFIGURATION */
#define FLASH_STORAGE_BASE_SIZE (0x10000) /* 64 KB for FlashDB */
/* 2. FIXED SIZES & OFFSETS */
#define _FIXED_BL2_OFFSET_SIZE (FLASH_AREA_BL2_NOHDP_OFFSET + FLASH_AREA_BL2_NOHDP_SIZE)
#define FLASH_S_PARTITION_SIZE (0x18000)
/* 3. DYNAMIC SIZES */
#define _RAW_APP_SPACE (FLASH_TOTAL_SIZE - _FIXED_BL2_OFFSET_SIZE - FLASH_STORAGE_BASE_SIZE)
#define _ALIGN_STEP (FLASH_AREA_IMAGE_SECTOR_SIZE * 2)
#define _ALIGNED_APP_SPACE (_RAW_APP_SPACE - (_RAW_APP_SPACE % _ALIGN_STEP))
/* Swap mode partitions calculation */
#define FLASH_STORAGE_SIZE (FLASH_STORAGE_BASE_SIZE + (_RAW_APP_SPACE - _ALIGNED_APP_SPACE))
#define _HALF_APP_SPACE (_ALIGNED_APP_SPACE / 2)
#define FLASH_NS_PARTITION_SIZE (_HALF_APP_SPACE - FLASH_S_PARTITION_SIZE)My questions:
- When modifying the partition sizes and boundaries in flash_layout.h using a Single Image (MCUBOOT_APP_IMAGE_NUMBER = 1), do I need to manually update erase_vect, write_vect, or secure_vect in SBSFU_Boot/Src/low_level_device.c?
- Are there specific TrustZone (SAU/MPU) alignments required for the SCRATCH area that I might have broken with my dynamic calculation?
- What is the recommended way to resolve the status write fails in Swap mode for a custom flash layout on STM32U5?
Thank you in advance for your help!