Skip to main content
Associate II
Dec 24, 2025 6:00 AM UTC
Solved

STM32U3: RDP Level 1: Flash read access and debugging behavior

Hello,

I would like clarification on the behaviour of STM32U3 devices when Readout Protection (RDP) Level 1 is enabled.

Configuration:

  • TrustZone: Disabled

  • Debug interface: SWD/JTAG

Questions:

  1. With RDP Level 1, is Flash completely unreadable by any third-party tool or by any boot mode (system memory boot, RAM boot, etc.), except when accessed by application code running on the MCU?

  2. With RDP Level 1, is application debugging still supported (attach debugger, halt, step, breakpoints), and are there any known limitations compared to RDP Level 0?

Any confirmation or documentation reference would be appreciated.

Thank you,
Vijay

TDK
TDKBest answer
Dec 24, 2025 3:00 PM UTC

1) If you start the chip normally and it boots to user flash, the user program can access flash but the debug interface cannot.

TDK_0-1766587683257.png

2) STM32CubeIDE won't be able to debug in RDP 1 in my experience. It may be technically possible but the workflow hasn't been set up with that in mind.

Typically development is done in RDP 0 and RDP 1 is set when the program is finished.

"If you feel a post has answered your question, please click ""Accept as Solution""."

1 reply

TDK
TDKBest answer
Dec 24, 2025 3:00 PM UTC

1) If you start the chip normally and it boots to user flash, the user program can access flash but the debug interface cannot.

TDK_0-1766587683257.png

2) STM32CubeIDE won't be able to debug in RDP 1 in my experience. It may be technically possible but the workflow hasn't been set up with that in mind.

Typically development is done in RDP 0 and RDP 1 is set when the program is finished.

"If you feel a post has answered your question, please click ""Accept as Solution""."