Associate II
Oct 4, 2021 2:39 PM UTC
Question
STM32L433RC SBSFU "Fw header authentication error"
- 2 replies
- 2466 views
Hello,
I am trying to run the Secure boot feature on STM32L433RC using the SBSFU library example project (single image slot). The example project I am modifying is STM32L432KC board.
Below are the modification/steps I made to example project to run on STM32L433RC:
- change the UART GPIO pins.
- change the LED GPIO pins.
- Disabled all the protections for now.
- Compiled SECore, SBSFU and User app.
- Downloaded the SBSFU to STM32L433RC.
- Opened Tera Term, Hit reset button.
- When asked to send the file using YMODEM protocol, I selected the SBSFU_UserApp.bin and the below error in the image is getting triggered.
Can anyone help me to successfully load the User app onto the board? Please let me know if I need to modify anything more or change the above modifcations.
Thanks!