Skip to main content
Rekha.k
Associate II
Jun 13, 2019 1:00 PM UTC
Question

STM32L1xxx Hardware CRC calculation

I am working on STM32L151QD MCU. I want to implement CRC feature in my application using STM hardware CRC block.

i am trying below steps to configure HW CRC:

uint32_t crc;

 uint32_t t_buffer[4] = {1,2,3,4};

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_CRC, ENABLE);  

  //Reset HW CRC 

   CRC_ResetDR();

  crc = CRC_CalcBlockCRC(t_buffer, sizeof(t_buffer));

  printf("hw crc = %d\n", crc);

  if ( CRC_GetCRC() != crc)

  {

   printf("error in HW CRC\n");

  }

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_CRC, DISABLE); /* Turn OFF CRC */

  return crc;

But every time HW computed CRC is different even if the input buffer is same all the time.

am i missing anything?

anything else to be configured to get correct CRC ?

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
Jun 13, 2019 1:17 PM UTC

Isn't the length parameter a word count, not a byte count?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Rekha.k
Rekha.kAuthor
Associate II
Jun 13, 2019 1:40 PM UTC

Hi there was a mistake. in code i am passing word count only. and i was debugging the code. i understood why i was getting different CRC everytime.

I have to reset DR register - CRC_ResetDR() during start of every computation.

Thanks