Skip to main content
Associate III
November 14, 2025
Question

STM32H7Sx - Passing volatile data to lower HDPL levels

  • November 14, 2025
  • 2 replies
  • 183 views

On a secured STM32H7Sx device (in CLOSED or LOCKED product state), what is the recommended way of passing volatile data to lower HDPL levels?

According to the reference manual, the SBS_RSSCMDR register can be used to pass volatile data from HDPL 1, 2 or 3 to HDPL 0 (RSS), so that part of the answer is covered:

Bits 15:0 RSSCMD[15:0]: RSS command
The application can use this bitfield to pass on a command to the RSS, executed at the
next reset.

But what if you want to pass volatile data from HDPL 2 or 3 to HDPL 1?
(E.g., HDPL 2 wants to call into HDPL 1 so HDPL 2 first needs to write some volatile command somewhere, then execute a reset, then HDPL 0 (RSS) boots, then HDPL 1 boots and picks up the volatile command from somewhere.)
SBS_RSSCMDR cannot be used because RSS will interpret this value as well, and RSS might clear this value at the moment it boots HDPL 1.

2 replies

Jocelyn RICARD
ST Employee
December 3, 2025

Hello @Eliasvan ,

this mechanism is not provided to be used in normal application as far as I know. It is used to launch a RSS command.

You can use specific location of RAM to transmit information from application to secure boot.

Secure boot have to avoid initialization of this specific location.

Best regards

Jocelyn

EliasvanAuthor
Associate III
June 24, 2026

Dear Jocelyn,

Thank you for your answer!

In order for me to fully accept your answer, I would need to know what location of RAM I can use without RSS wiping it, can you provide me this?

Thanks again!