Skip to main content
Explorer
May 20, 2025 9:09 AM UTC
Question

STM32H7S7: Configure OSPI + MCE

Hi,

I am using the STM32H7S78-DK. I want to upload an encrypted application to the external 1-Gbit Octo-SPI flash memory connected to XSPI2.

I am using the explanation in this video: https://www.youtube.com/watch?v=JxhKmVUB2Ws&list=PLnMKNibPkDnFQXYK0ztHV9iMVS6EAtKpD&index=10

as well as the example code linked in the video description: https://github.com/ST-TOMAS-Examples-ExtMem/stm32h7rs_ospi_mce?tab=readme-ov-file

 

As I am using XSPI2, I configure MCE2 to use the Noekeon encryption. My code looks like this:

MCE_HandleTypeDef hmce2;

uint32_t Key[4]= {0x23456789, 0xABCDEF01, 0x23456789, 0xABCDEF01};



hmce2.Instance = MCE2;

if (HAL_MCE_Init(&hmce2) != HAL_OK){

Error_Handler();

}

{

MCE_NoekeonConfigTypeDef NoekeonConfig ;

MCE_RegionConfigTypeDef RegionConfig ;

NoekeonConfig.KeyType = MCE_USE_MASTERKEYS;

NoekeonConfig.pKey = Key;

if (HAL_MCE_ConfigNoekeon(&hmce2, &NoekeonConfig) != HAL_OK){

Error_Handler();

}

/* Set the MCE Region configuration*/

RegionConfig.Mode = MCE_BLOCK_CIPHER;

RegionConfig.ContextID = MCE_CONTEXT1;

RegionConfig.StartAddress = 0x70000000;

RegionConfig.EndAddress = 0x78000000;

RegionConfig.PrivilegedAccess = MCE_REGION_NPRIV;

RegionConfig.AccessMode = MCE_REGION_READWRITE;

if (HAL_MCE_ConfigRegion(&hmce2, MCE_REGION1, &RegionConfig) != HAL_OK){

Error_Handler();

}

}

The application runs properly on the external flash as long as I do not use the MCE.

As soon as I use the MCE configuration above (in the external loader and the bootloader), I end up in the HardFault_Handler.

 

Is there anything wrong or missing in my MCE configuration?

Thanks for any help!

 

This topic has been closed for replies.

1 reply

Billy OWEN
ST Employee
May 21, 2025 3:35 PM UTC

Hi @katja 

 

This post has been escalated to the ST Online Support Team for additional assistance.  We'll contact you directly.

 

Regards,

Billy