Skip to main content
Associate
September 24, 2026
Question

STM32H7RS Debug Authentication Failed – Timeout while receiving response after signing token

  • September 24, 2026
  • 1 reply
  • 33 views

Hello ST Community,

I am working with an STM32H7S78-DK board and trying to perform Debug Authentication using STM32CubeProgrammer v2.21.0.

The Discovery sequence succeeds successfully, and the target is detected correctly. However, the Debug Authentication fails after selecting the required permission.

Environment

  • Board: STM32H7S78-DK
  • STM32CubeProgrammer: v2.21.0
  • SDM Library: v1.2.0
  • SDA version: 2.0.0
  • PSA lifecycle: ST_LIFECYCLE_CLOSED
  • PSA authentication version: 1.0
  • Cryptosystem: Ecdsa-P256 SHA256
  • Key: Keys/key_3_leaf.pem
  • Certificate: Certificates/cert_leaf_chain.b64
  • Password: Binary/password.bin

Discovery result

The discovery command completes successfully

      -------------------------------------------------------------------
                       STM32CubeProgrammer v2.21.0
      -------------------------------------------------------------------


Start Debug Authentication Sequence

Open SDM Lib
SDMOpen                       :   624 : open       : SDM API v1.0

SDMOpen                       :   625 : open       : SDM Library version v1.2.0

open_comms                    :   513 : open       : Asserting target reset

open_comms                    :   517 : open       : Writing magic number

open_comms                    :   537 : open       : De-asserting target reset

open_comms                    :   584 : open       : Communication with the target established successfully

response_packet_lock
discovery: target ID.......................:0x485
discovery: SoC ID..........................:0x00000000_34323433_3034510B_00270059
discovery: SDA version.....................:2.0.0
discovery: Vendor ID.......................:STMicroelectronics
discovery: PSA lifecycle...................:ST_LIFECYCLE_CLOSED
discovery: PSA auth version................:1.0
discovery: ST HDPL1 status.................:0xa
discovery: ST HDPL2 status.................:0xa
discovery: ST HDPL3 status.................:0x0
discovery: Token Formats...................:0x200
discovery: Certificate Formats.............:0x201
discovery: cryptosystems...................:Ecdsa-P256 SHA256
discovery: ST provisioning integrity status:0xeaeaeaea
discovery: permission if authorized...........:(a/14) ==> Full Regression
discovery: permission if authorized...........:(b/2) ==> Level 3 Intrusive Debug
discovery: permission if authorized...........:(c/1) ==> Level 2 Intrusive Debug
discovery: permission if authorized...........:(d/0) ==> Level 1 Intrusive Debug
discovery: permission if authorized...........:(e/127) ==> Forced Download
To select multiple permission/actions:
    Using numerical values: List the needed bit numbers, separated by commas without spaces.
    Using symbolic letters: List the needed letters by concatenating them without separators.

Debug Authentication: Discovery Success

      -------------------------------------------------------------------
                       STM32CubeProgrammer v2.21.0
      -------------------------------------------------------------------

Key file path submitted : Keys/key_3_leaf.pem

Certificate file path submitted : Certificates/cert_leaf_chain.b64

Password file path submitted : Binary/password.bin


Start Debug Authentication Sequence

Open SDM Lib
SDMOpen                       :   624 : open       : SDM API v1.0

SDMOpen                       :   625 : open       : SDM Library version v1.2.0

open_comms                    :   513 : open       : Asserting target reset

open_comms                    :   517 : open       : Writing magic number

open_comms                    :   537 : open       : De-asserting target reset

open_comms                    :   584 : open       : Communication with the target established successfully

response_packet_lock
discovery: permission if authorized...........:(a/14) ==> Full Regression
discovery: permission if authorized...........:(b/2) ==> Level 3 Intrusive Debug
discovery: permission if authorized...........:(c/1) ==> Level 2 Intrusive Debug
discovery: permission if authorized...........:(d/0) ==> Level 1 Intrusive Debug
discovery: permission if authorized...........:(e/127) ==> Forced Download
SDMOpen                       :   624 : open       : SDM API v1.0

SDMOpen                       :   625 : open       : SDM Library version v1.2.0

open_comms                    :   513 : open       : Asserting target reset

open_comms                    :   517 : open       : Writing magic number

open_comms                    :   537 : open       : De-asserting target reset

open_comms                    :   584 : open       : Communication with the target established successfully

 

After discovery, I run Debug Authentication with the key, certificate chain and password.

The authentication reaches the token-signing stage:

[00%]   discovery command
[10%]   sending discovery command
[20%]   receiving discovery
response_packet_lock
[40%]   loading credentials

Keys/key_3_leaf.pem

Certificates/cert_leaf_chain.b64
[50%]   sending challenge request
[60%]   receiving challenge
response_packet_lock
[70%]   signing token
Please select the possible permission/actions:

(a/14) Full Regression

(b/2) Level 3 Intrusive Debug

(c/1) Level 2 Intrusive Debug

(d/0) Level 1 Intrusive Debug

(e/127) Forced Download
a

 the submitted permissions are : a
SDMAuthenticate               :  1391 : client     : Found 3 certificates

response_packet_lock
Timeout while receiving response...
SDMAuthenticate               :  1415 : client     : Unexpected response status 3

Issue

The target communication is established successfully and the Discovery command works. The credentials are also loaded and 3 certificates are found.

However, immediately after submitting permission a (Full Regression), the target does not provide the expected response:

Timeout while receiving response...
Unexpected response status 3

I have also tried the procedure multiple times, but I consistently get the same authentication failure.

Could someone please help me understand:

  1. What does Unexpected response status 3 indicate in this Debug Authentication sequence?
  2. Why would Discovery succeed but authentication fail after the token is signed?
  3. Could this be related to the certificate chain, key/certificate provisioning, password, lifecycle state, or provisioning integrity status 0xeaeaeaea?
  4. Is there any additional provisioning or configuration step required before Debug Authentication can successfully authorize Full Regression?
  5. Are there any specific reset timing requirements for STM32H7RS during the authentication sequence?

I would appreciate any guidance on how to identify the exact cause of the authentication failure.

Thank you.

1 reply

Frantz LEFRERE
ST Technical Moderator
September 24, 2026

Dear ​@Kshor,
first, I would advise to use the last CubeProgrammer version 2.23

have you done any modification on your DK board ?
In past we have seen this kinf error message when the MCU reset was not driven during the debug authentication ( usually when people use an external stlink and miss to connect the RST pin). 


How have you provisioned your board ? With which obk file ?


I did a quick test with STM32CubeProgrammer v2.21.0. and DK no issue seen ( but I only have version with SDA version.....................:1.0.0) 

I have provisionned the board with default DA from cube programmer and the use this command :

cd C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin
STM32_Programmer_CLI.exe -c port=SWD speed=fast per=a key=.\DA_Default_Config\STM32H7RS\key_3_leaf.pem cert=.\DA_Default_Config\STM32H7RS\cert_leaf_chain.b64  debugauth=1

Best regards,

Frantz