Skip to main content
Visitor II
Oct 28, 2026 8:25 AM UTC
Question

STM32H755ZI-Q NUCLEO Board Inaccessible After Enabling Secure Memory Area

I am working on a secure bootloader implementation for the STM32H755 microcontroller using the NUCLEO-H755ZI-Q development board.

I am facing an issue where the MCU has become inaccessible after configuring the secure memory area through option bytes. I would appreciate your guidance on recovering the device.

Hardware and software details

  • Board: NUCLEO-H755ZI-Q
  • MCU: STM32H755
  • STM32CubeProgrammer: Version 2.20.0
  • Debug probe: Onboard ST-LINK V3
  • RDP: 0xAA (Level 0)
  • SECURITY: Enabled
  • SEC_AREA_START1: 0x000
  • SEC_AREA_END1: 0x1FF (128 KB secure area)

Sequence of events

  1. I erased the user flash before configuring the secure memory area, so the bootloader firmware was no longer present.
  2. I enabled the SECURITY option byte and configured a 128 KB secure area from 0x08000000 to 0x0801FFFF.
  3. After applying the option-byte configuration, I could no longer connect to the MCU.
  4. The RDP level remains 0xAA (Level 0). I have not intentionally changed it to Level 1 or Level 2.

Recovery attempts

I have tried the following without success:

  • ST-LINK connection using SWD.
  • Connection under reset and Hot Plug modes.
  • Reduced SWD frequency.
  • Entering System Memory boot mode using BOOT0 (LD3 is not glowing).
  • Connecting through the UART ROM bootloader on COM13 at 115200 baud.
  • Tried with all available connection modes using cube programmer.

The ST-LINK connection reports errors such as “Unable to get core ID” and “No STM32 target found.” The UART connection fails during device activation with a timeout waiting for acknowledgement.

I also reviewed the STM32H755 reference manual and found the documented mass-erase-with-protection-removal procedure. However, because the MCU is inaccessible and the bootloader has already been erased, I currently have no way to execute the required recovery firmware on the target.

Request for assistance

Could you please advise on the officially supported recovery procedure for this condition?

Specifically, I would like to know:

  1. Is it possible to recover the MCU while RDP remains at Level 0 and the secure memory area is enabled?
  2. Is there a supported method to execute the protection-removal or mass-erase sequence when both SWD and the ROM bootloader are inaccessible?
  3. Can the secure-area configuration be removed through any supported ST-LINK, STM32CubeProgrammer, or factory recovery procedure?
  4. If recovery is not possible through the available interfaces, is there another recommended solution?

 

My intention is to secure the bootloader code for a production implementation, and I would like to understand the correct procedure before enabling this feature again on another board.

Please let me know if you require the option-byte configuration screenshots, connection logs, or any additional information.

1 reply

Jocelyn RICARD
ST Employee
Oct 29, 2026 6:15 PM UTC

Hello ​@sneham ,

I’m not sure to understand why you made this steps like this.

As soon as a secure memory is created, the JTAG is disabled. So, even in RDP Level 0 you will not be able to access to the device.

You can see the mechanism described in the RM0399 in chapter 5 Secure memory management.

I share an old example probably already shared in another post

It is supposed to be run on Nucleo STM32H755 and provides interactive menu to enable and disable protections.

It may need some updates but you have the information

Best regards

Jocelyn