Skip to main content
Roger, Huang
Associate
Feb 3, 2021 10:23 AM UTC
Solved

STM32H750VBT6 access crypt registers all read back zero

Hi,

Developing AES GCM on a customer board that is used STM32H750VBT6 with CubeMX 6.1.1 has a problem needs help.

Tested example code CRYP_AES_GCM from STM32Cube_FW_H7_V1.8.0 Projects/STM32H735G-DK/Examples/CRYP is failed. And used JLINK debug figure out all registers of crypt are all zero. and test code run to DES cipher.

Has any suggestion?

Thanks

This topic has been closed for replies.
Tesla DeLorean
Tesla DeLoreanBest answer
Guru
Aug 10, 2021 8:33 PM UTC

Official word is that 2020 Week 22 thru 47 are impacted.

https://community.st.com/s/question/0D53W000010RpinSAC/how-to-enable-the-stm32h750vbt6-hw-crypto

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..

18 replies

Tesla DeLorean
Guru
Feb 3, 2021 11:22 AM UTC

Check that the clock is enabled in the RCC and any secondary clocks or PLLs it might need. Check also HASH unit.

​

A​ttach a photograph of the IC top markings. Clear and in focus.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Roger, Huang
Associate
Feb 3, 2021 12:32 PM UTC

0693W000007Dm9jQAC.png0693W000007Dm9UQAS.pngTesla,

Thank your great help.

After checked HASH is also read back zero and both can not modified any bit of their registers.

I also checked RCC registers too CLK of HASH, CRPY are both enabled, but only PLL1 is enabled and stable.

Roger, Huang
Associate
Feb 5, 2021 12:49 AM UTC

@Community member​ 

I'm stuck with this issue. Could you share more clues to let me try?

BR

Roger, Huang

Tesla DeLorean
Guru
Feb 5, 2021 1:37 AM UTC

Check the soldering in the low right.

Do you have a USART wired on the board that can be used to output diagnostic output? Define USART and PINS

What HSE frequency are you using?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Roger, Huang
Associate
Feb 5, 2021 6:23 AM UTC

It has featur 2 USARTs​, and uses SWO for debug print.

And no SHE, use SHI for system clock.

SHI now is configured 64MHz

The system clock has been tested 480, and 240MHz​

Lulo
Visitor II
Apr 16, 2021 5:11 PM UTC

Hello,

I have the same issue with the same chip in the same revision STM32H750VBT6 rev_V. CRYP registers remain 0 even with the last update of HAL drivers. Other functions are OK.

The code works well with another board with an older revision STM32H750VBT6 rev_Y.

It seems that tools do not manage correctly rev_V.

I'm stuck. Is there a change or an update to apply to make it work with the last (and now only) chip revision available?

Pavel A.
Apr 16, 2021 5:58 PM UTC

Below is a small test that we use to distinguish H753 from H743. H750 is similar to 753, so this should work on that too,

#ifndef STM32H753xx
#define STM32H753xx /* override! */
#undef STM32H743xx
#endif
 
#include "stm32h7xx_hal.h"
#include <stdbool.h>
 
// Test if the STM32H7 crypto is actually working,
// so this is H7 variant with crypto (ex. H753 vs H743)
// Check that CR regster of HASH or CRYP holds written value
bool H7_hw_crypto_test()
{
 // Test if HASH->CR is writable
 __HAL_RCC_HASH_CLK_ENABLE();
 HAL_Delay(5);
 HASH->CR = 0;
 __DSB();
 HASH->CR = 0x20; // set HASH_CR_DATATYPE=HASH_DATATYPE_8B
 __DSB();
 uint32_t u = HASH->CR;
 bool y = ((u & 0x30) == 0x20);
 
 if (!y) {
 __HAL_RCC_HASH_CLK_DISABLE();
 }
 return y;
}

Tesla DeLorean
Guru
Aug 6, 2021 7:42 PM UTC

@Pavel A.​  thanks for posting that

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Lulo
Visitor II
Apr 19, 2021 12:36 PM UTC

Thank you for the test code. I have tried it. I confirm that it returns "false" for the chip in rev V, and that all HASH and CRYP registers return always zero. Here is a picture of this chip:

0693W000008zx1WQAQ.jpgOn an older chip in rev Y, the test code return "true" and both HASH / CRYP registers have correct values. For example, CRYP->SR is correctly initialised at 0x3. Here is a picture of this older chip that works perfectly:

0693W000008zx54QAA.jpg 

Do I have to conclude that my chip in rev V does not provide the hardware HASH and CRYP functions?

Both chip are H750 versions, and according to datasheet should feature these functions.

Roger, Huang
Associate
Jun 11, 2021 2:25 AM UTC

Update: tested on CubeMX 6.2.1 , MCU package 1.9.0: Makefile generation

  1. Date code : 051 is work as register accessible.
  2. Data code: 036 is failed to access register. checked by verify program, and STM32CubeProgrammer both.

Could have any input?