jiangpenAssociate III5 years agoSep 13, 2021 1:13 AM UTCQuestionSTM32H7 cannot program anymore after running example of SBSFU example (1 Image) for STM32H7B3.2 replies1803 viewsthe stm32programmer can connect, erase whole chip, but cannot program.What I have done is to run example of SBSFU example (1 Image). I can see bootloader running. Then I try to erase the chip to program my other program.I try to load the PCROP and secure section from my coworker's setting, but it does not allow me to change.I attached all the stm32programmer logs.May I know anyway can solve this lock program, or this device is actually lockedprogram1.logSTM32CubeProgrammerSTM32H7 seriesSBSFU